I cannot see the result data more than 2500 points in Measure Result Dialogue.
Question:
I believe that the instrument supports the measurement data up to 100,000 points.
However, I cannot see the result data more than 2500 points in Measure Result Dialogue. Question:
I believe that the instrument supports the measurement data up to 100,000 points.
However, I cannot see the result data more than 2500 points in Measure Result Dialogue. Why?
Answer:
The instrument may be configured to use the conventional command set designed for using the existing programs which you created to control existing instruments such as Keithley 2400.
Keithley 2400 doesn't support the sweep measurement including more than 2500 measurement points so that you can't see the result data more than 2500 points.
Please take the actions described in the material below and configure the instrument to use the default command set which supports all the B2901/02/11/12A functions.