What is the size of the internal user memory on the handheld spectrum analyzer? How many trace files or pictures can be saved?
The internal user memory of the HSA holds up to 60 MB. If a user saves the trace data as *.csv (approximately 18 kB per file), the HSA could save more than 3000 files. If the user saves the trace data as *.trc (approximately 5 kB per file), the HSA could save more than 1000 files.