Starting Download..
save Save

Why will the counter not make low frequency measurements?

Verify the System Timeout setting by pressing Utility - Instr Setup - Time Out Settings. Turn the time out off or set it to a value much greater than the period of the signal (e.g. 10s). The system time out prevents the counter from hanging should the measurement fail to complete. A value of 9.91E+37 is returned for the incomplete measurement and the next measurement begins. The system time out is turned off when the counter is shipped from the factory.
 

Was this helpful?


Didn't find what you're looking for?