Flyers
Procedure overview
In this demo…
Required Instrument and fixture
E5061B-115/135/215/235 or E5061BEP-115/235
(also E5061B-117/137/217/237 available for 75 Ω DUT)
1. Connect DUT to E5061B
2. Set measurement parameters
a. Press [Preset] then press OK
b. Set Frequency
Press [Center] then enter 1.09 GHz
Press [Span] then enter 200 MHz
c. Set measurement traces
Press [Display] then press Num of traces, and 2
Press Allocate Traces and x2
d. Set measurement parameters for trace2
Activate trace2
Press [Meas] then press S21
Press [Scale] then press Auto Scale All
e. Set IFBW
Press [Avg] then enter 1 kHz
3. Perform calibration (Mechanical Cal)
a. Select calibration kit and calibration type
Press [Cal] then press Cal Kit, and press 85032B/E
Press Calibrate, then press Enhanced Response
b. Measure calibration standard
Connect open std. to port1 then press Open
Connect short std. to port1 then press Short
Connect load std. to port1 then press Load
Connect thru std. between port1 and port2 then
press Thru
c. Activate calibration
Press Done
4. Measure the insertion loss
a. Connect DUT to E5061B if you performed calibration
b. Display marker on peak of the S21 measurement
Activate trace2, then press [Marker]
Press [Marker Search] then press Max
c. Measure the marker value displayed as shown in the figure below. In this example, the response value denotes the insertion loss.
5. Measure the bandwidth parameters
a. Perform bandwidths search
Press [Marker Search] then press Bandwidth
b. The bandwidth data items (BW, cent, low, high, Q, loss) is displayed as shown in the figure below.
Additional Demo: Bandwidth limit test
The test result of the trace can be indicated in the upper[1]right section of the graph.
a. Bandwidth test setup
Press [Analysis] then press Bandwidth Limit
Press [Min Bandwidth] then enter smaller value
than actual bandwidth
Press [Max Bandwidth] then enter grater value than
actual bandwidth
b. Turning on the bandwidth limit test function
Press BW Test
×
Please have a salesperson contact me.
*Indicates required field
Thank you.
A sales representative will contact you soon.