Column Control DTX

W1918 LTE-Advanced Baseband Verification Library

Data Sheets

Offering the Fastest Path from Algorithms to R&D Verification

The W1918 LTE-Advanced Baseband Verification Library saves time, reduces engineering effort and accelerates the maturity of 4G baseband PHY designs for next-generation 3rd Generation Partnership Project (3GPP) Long Term Evolution LTE-Advanced systems. It enables system architects, algorithm developers and baseband hardware designers to investigate, implement and verify their Layer 1 signal processing designs in the presence of meaningful RF and test signals. The library gives the user piece of mind that a physical layer (PHY) meets or exceeds real-world performance requirements from the European Telecommunications Standards Institute (ETSI).

The W1918 LTE-A Baseband Verification Library is a Layer 1 simulation reference library option for Keysight SystemVue. The blockset, reference designs, and test benches assist the design and verification of next-generation communication systems, by providing configurable physical layer waveforms and data for 3GPP Releases 8/9 (LTE) and 10-13 (LTE-Advanced). The library is useful for simulation-based exploration of challenging algorithms, up to 8x8 MIMO throughput verification, and can be easily integrated with Keysight signal sources and analyzers.

Features

  • Working simulation-based baseband reference designs for UE & eNodeB
  • Open, parameterized block diagrams allow exploration and customization inside the signal processing chain
  • Compare your internal test vectors against a trusted IP reference
  • Use Keysight simulation blocks to:Supply missing functions/models
  • Create complete Layer 1 scenarios
  • Add MIMO, fading, interferences
  • Simulate BER/Throughput
  • Interoperate with real test

Configuration

The W1918 LTE-Advanced Baseband Verification Library can be added as an option to any SystemVue environment or bundle.

The W1918 LTE-A library is a superset of the W1910 LTE library, and includes it. It adds algorithm models for LTE-Advanced, making a complete library that supports 3GPP releases 8-13, including Narrowband Internet of Things (NB-IoT).

The W1918 library is itself included in the W1907 5G Forward Verification Library Bundle, along with modelsets for 2G, 3G, MIMO Channel, and the new pre-5G library. If you are considering moving toward 5G, then the W1907 bundle is an excellent value, assisting compatibility across multiple generations of standards, not just 4G.

The W1918 is especially well-suited to work with other SystemVue libraries, such as the W1715 MIMO Channel Builder, the W1716 Digital Pre-Distortion Builder. It can also be used by system architects to customize test benches for use with Keysight ADS VTB personalities: W2388 LTE VTB (LTE only), W2390 LTE-A VTB (LTE-A only, not including LTE). Finally, the W1918 LTE-A library interoperates with Keysight Signal Studio personalities for LTE- A (N7624B, N7625B), as well as Keysight 89600 VSA personalities 89601B-BHG and 89601-BHH.

C++ source code for the W1918 LTE-A library is available as a premium service product “W1912BEL Baseband Exploration Library”.

×

Please have a salesperson contact me.

*Indicates required field

Preferred method of communication? *Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By clicking the button, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you.

A sales representative will contact you soon.

Column Control DTX