What external mixers will work with my PXA/mmW EXA and how do I order them?
Currently, the N9030A PXA/mmW EXA with Option EXM will work with either the 11970 Series (with the exception of the 11970K) or OML Inc. (formerly Oleson Microwave Lab) mixers. Keysight is adding a new line of mixers specifically for use with PXA/mmW EXA as well - for more information about these new mixers, go to http://www.agilent.com/find/smartmixers
Note: The 11970 Series mixers will require the use of an external diplexer with the PXA mmW EXA. The following table provides information about ordering OML mixers (through Keysight) for frequencies up to 325 GHz, which are optimized for the PXA/mmW EXA.
N9029AE03 | Ordering convenience for one OML WR-03 (220 to 325 GHz) OML harmonic mixer |
N9029AE05 | Ordering convenience for one OML WR-05 (140 to 220 GHz) OML harmonic mixer |
N9029AE06 | Ordering convenience for one OML WR-06 (110 to 170 GHz) OML harmonic mixer |
N9029AE08 | Ordering convenience for one OML WR-08 (90 to140 GHz) OML harmonic mixer |
N9029AE12 | Ordering convenience for one OML WR-12 (60 to 90 GHz) OML harmonic mixer |
N9029AE13 | Ordering convenience for one OML INC. LO/IF diplexer with cables and adapter |
The N9029AE13 is the diplexer required for use with Keysight 11970 Series mixers with PXA.