Do the 1000 Series oscilloscopes provide the ability to switch off the Auto Scale feature?
You cannot do this on the front panel. However, there are remote interface SCPI commands for the 1000 Series oscilloscopes that enable or disable the front panel Auto Scale function.
The commands are:
- AUToscale:DISable (disables Auto Scale)
- AUToscale:ENABle (enables Auto Scale)
The enable/disable is kind of a permanent setting until it is reprogrammed, as it flips the bit on the non-volatile memory on the oscilloscope.