Starting Download..
save Save

Can I use PXI-1 existing cards in the Keysight Card cages and are there any that will no longer work?

Older PXI (PXI-1) modules (which have a J2 present) will not work in Keysight 18-slot PXIe chassis. It may be possible to modify the PXI-1 module to work in the 18-slot PXIe chassis by replacing the J2 connector with an xJ4 connector. Per the PXI specifications, when a J2 connector is replaced with an xJ4 connector, most of the local bus lines are no longer available. However, few modules have used the local bus.

Was this helpful?


Didn't find what you're looking for?