On the ENA / ENA-L, it appears as though only the first channel is activated. Is this normal?
(SUPPORTED MODELS IN BOLD: E5071C E5070B/71B E5070A/71A E5061A/62A E5061B E5072A)
Yes, this is normal operation.
On the ENA / ENA-L, when configured with multiple channels, the default trigger mode of channel 1 is set to CONTINUOUS,
while all other channels are set to HOLD. To activate additional channels, first select the desired measurement channel and then
select the STIMULUS - TRIGGER keys and set the trigger mode to CONTINOUS.