Choose a country or area to see content specific to your location
- Home
- Software Details
- Software Details
What are you looking for?
Suggested searches
No product matches found - System Exception
Matched content
N67xx Mainframe Digital Ports
This is an example program that works with the following Model Numbers:
- N6700B
- N6701A
- N6702A
- N6705A
- N6705B
The attached files contain an example of how set up the 8 pin digital port on the Keysight N67xx DC Power mainframes. This program allows the user to set the function, the polarity, the fault conditions, read the digital input, and set the digital output.
There are two attached files. One is a compiled exe file that will run on any PC with the Keysight IO Libraries. The second is a Visual Basic 6 program that includes all of the underlying code. This code is free to modify.
Please e-mail any feedback on this example to plsp-power_prod_support@keysight.com
Microsoft is a U.S. registered trademark of Microsoft Corporation.