Column Control DTX

Young’s Modulus of Dielectric ‘Low-k’ Materials

Application Notes

In digital circuits, insulating dielectrics separate the conducting parts (wire interconnects and transistors) from one another. As components have scaled and transistors have gotten closer and closermtogether, the insulating dielectrics have thinned to the point where charge build up and crosstalk adversely affect the performance of the device. It is this reduction in scale which drives the need for insulating materials with lower dielectric constant. A ‘low-k’ material is one with a small value for dielectric constant relative to silicon dioxide (SiO2)—a former dielectric of choice. The dielectric constant of SiO2 is 3.9. This number is the ratio of the permittivity of SiO2 divided by permittivity of vacuum, eSiO2/∈0,where ∈0 = 8.854 x 10-6 pFμm. There are many materials with lower dielectric constants, but few of them can be suitably integrated into a semiconductor manufacturing process[1].

×

Please have a salesperson contact me.

*Indicates required field

Preferred method of communication? *Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By clicking the button, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you.

A sales representative will contact you soon.

Column Control DTX