Agilent Technologies

Voltage Scan and Plot of Data: 34970A/72A (IVI -- LabView)

This program sets the 34970A/72A for a single scan of DC voltage and plots the results on a graph.

NOTE: National Instruments has a G Driver for the 34970A that can be used with the 34972A as well. Simply set the "ID Query" input of the "Initialize.vi" to "False" to use the 34970A LabView driver with the 34972A. See our FAQ on this topic for illustrations on how to do this.

The 34970A LabView G Driver, and examples using it, can be obtained from the National Instruments web site at: www.ni.com

This example program requires LabView revision 8.5 or greater, and Agilent 34970A IVI driver revision 1.3.5.0 or greater.

LabView is a registered trademark of National Instruments Corporation

Copyright © 2010 Agilent Technologies Inc. All rights reserved.

You have a royalty-free right to use, modify, reproduce and distribute these example files (and/or any modified version) in any way you find useful, provided that you agree that Agilent has no warranty, obligations or liability for any Sample Application Files.

Agilent Technologies will not modify the program to provide added functionality or construct procedures to meet your specific needs.


© Agilent 2000-2010