Is there any special setting that I need to do in Keysight VEE before using the U2300A or U2500A DAQ with it?
Yes. In fact it is the most important thing you need to set before using the DAQ with Keysight VEE. As most instruments uses MSB byte ordering, DAQ utilizes LSB byte ordering instead and it is one of the most common problem we see when users are unable to obtain proper acquisition through the DAQ.
To set the byte ordering correctly, simply locate your DAQ via the Instrument Manager within VEE. Right click on your instrument and select 'Instrument Properties...'. Click on the 'Advanced...' button and you'll see the 'Advanced Instrument Properties' box appear. Under the 'General' tab, you'll see the 'Byte Ordering' is set to MSB by default. Simply change that to display LSB and you're done. Now, you're all set to start acquiring your data with VEE.