Why Can’t my PC Connect to my InfiniiVision Oscilloscope via its LAN/USB/GPIB Interface?
Troubleshooting
Summary
Troubleshooting for connecting InfiniiVision oscilloscope via its LAN/USB/GPIB interface.Question
Why can’t my PC connect to my InfiniiVision oscilloscope via its LAN/USB/GPIB interface?Answer
There are many ways to connect your InfiniiVision oscilloscope to your PC. If you are unable to connect to your PC, please ensure that the interface you are using is enabled on the oscilloscope. The PC will not see the scope if the interface is not enabled.To ensure that the interface is enabled, press the Utility button, then the I/O softkey, then the Control softkey. Use the Entry knob to select the interface you want to use, and press the Control softkey to toggle the interface on.