IO Libraries Suite: How do I install the E8491 driver when I upgrade from a previous release to IO Libraries Suite 15.1?
IO Libraries Revisions: Suite 15.1
The E8491 device driver will not install automatically if you upgrade from a previous release to IO Libraries Suite 15.1. This defect is fixed in IO Libraries Suite 15.5, which you can download at www.keysight.com/find/iosuite
Follow the instructions below, based on the operating system that your PC is running:
Windows Vista
- Copy the file:
C:\Program Files\Keysight\IO Libraries Suite\pnp\1394IPT.sys
to the following location:
C:\Windows\System32\drivers\1394IPT.sys - Open Windows Device Manager and navigate to the 'Other devices' category. Select the 'Unknown device' entry.
- From the Device Manager menubar, select 'Action', then 'Update Driver Software...'.
- In the wizard that appears, choose the option 'Browse my computer for driver software'.
- In the next screen, enter the location
C:\Program Files\Keysight\IO Libraries Suite\pnp
and click 'Next' - In the final screen that appears, click 'Close'.
- Open Keysight Connection Expert to view and configure the E8491.
Windows XP
- Copy the file:
C:\Program Files\Keysight\IO Libraries Suite\pnp\1394IPT.sys
to the following location:
C:\windows\system32\drivers\1394IPT.sys - Open Windows Device Manager and navigate to the 'Test & Measurement devices'. Select the 'Keysight E8491 1394 VXI controller' entry.
- From the Device Manager menubar, select 'Action', then 'Update Driver...'.
- In the Found New Hardware Wizard, select 'No, not this time', then click 'Next'.
- Select 'Install from a list or specific location (Advanced)', then click 'Next'.
- Enter the location
C:\Program Files\Keysight\IO Libraries Suite\pnp\
then click 'Next'. - On the final screen, click 'Finish'.
- Open Keysight Connection Expert to view and configure the E8491.
Windows 2000
- Copy the file:
C:\Program Files\Keysight\IO Libraries Suite\pnp\1394IPT.sys
to the following location:
C:\winnt\system32\drivers\1394IPT.sys - Open Windows Device Manager and navigate to the 'Test & Measurement devices' category. Select the 'Keysight E8491 1394 VXI controller' entry.
- From the Device Manager menubar, select 'Action', then 'Properties'. In the new window that appears, select the 'Driver' tab, then click 'Update Driver...'.
- In the wizard that appears, click 'Next'.
- Select the option 'Search for a suitable driver for my device', then click 'Next'.
- On the next screen, select 'Specify a location', then click 'Next'.
- Enter the location
C:\Program Files\Keysight\IO Libraries Suite\pnp\
then click 'OK'. - On the next screen, click 'Next'.
- On the final screen, click 'Finish'.
- Open Keysight Connection Expert to view and configure the E8491.
Last Updated: 01September, 2009