What is the limitation of the evaluation mode of the MWA software?
(SUPPORTED MODELS IN BOLD: E5071C E5072A E5070B/71B E5070A/71A E5061A/62A E5061B E5063A E5091A E5092A)
You can download the latest revision of the evaluation mode of the MWA software at: https://www.keysight.com/find/mwa
With this mode, the number of measurements with the MWA back-end application is limited according to trigger mode on the ENA. Doing further measurements with the MWA is not allowed.
Maximum 100 measurements (with manual or external trigger)
Maximum 500 measurements (with continuous trigger)
Note: There are no operational limitations for the evaluation mode of the front-end application.
Note: You can retrofit the software by the upgrade kit/product (E5070BU/E5071BU-790 for the E5070B/71B or E5005A for the E5071C) in order to enable full capability of the software.