Are there any step-by-step measurement examples for ENA 7 series?
(SUPPORTED MODELS IN BOLD : E5071C E5072A E5070B/71B E5070A/71A E5061A/62A E5061B E5063A E5091A E5092A)
Yes. There are some measurement examples in ENA help file. See following links for more detail.
[E5071C]
- Measurement Example of a Bandpass Filter
- Measuring the SAW Bandpass Filter Using the Segment Sweep
- Evaluating a Duplexer
- Measuring the Deviation from a Linear Phase
- Measuring an Unbalanced and Balanced Bandpass Filter
- Measuring Parameters with Cable
- Evaluating Transmission Characteristics of a Front End Module
- Executing Power Calibration
Also, quick start section in help file helps you to understand the E5071C basic operation.
[E5072A]
- Measurement Example of a Bandpass Filter
- Measuring the SAW Bandpass Filter Using the Segment Sweep
- Measuring the Deviation from a Linear Phase
- Measuring Parameters with Cable
- Executing Power Calibration
- Measuring Using Configuration Test Set
Also, quick start section in help file helps you to understand the E5072A basic operation.