When using a U2701A/U2702A USB Modular Oscilloscope, what is the maximum data point of the waveform that I can save ?
When using a U2701A/U2702A USB Modular Oscilloscope, you can save a maximum of 2000 data points for a single channel measurement. Normally, 1250 data points can be saved.
There are fix data points for the Time/Div Settings as below:
TIME/Div Setting | Data Point For Single Channel | Data Point For Dual Channel |
---|---|---|
500ns and above. | 1250 | 1250 |
200ns | 2000 | 1000 |
100ns | 1000 | 500 |
50ns | 500 | 250 |
20ns | 200 | 100 |
10ns | 100 | 50 |
5ns | 50 | 25 |
2ns | 20 | 10 |
1ns | 10 | 5 |