Column Control DTX

Inphi Delivers DDR Memory Interface Chip Using the ADS

Case Studies

Your Company

What types of products | Do you develop? | For what applications?

Inphi is a leading provider of memory interface chips. I’m product line manager for the Memory Interface Logic product line. The chip itself contains a PLL, decode logic and buffer logic running at 1.6 Gbps/pin in a 176 BGA package. Our products are used inside a DDR3-1600 RDIMM by our direct customers, the DRAM manufacturers. Our chip acts as an interface between the host controller, typically a microprocessor from Intel or AMD, and the DRAM chips inside the module. In turn, the modules are used inside high-end servers for the Internet and other data communications and data processing systems.

How do you work with other companies up and down the supply chain?

We work closely with the JEDEC consortium to deine the RDIMM topology standards and layout, but there is always some variation between each vendor’s implementation of what we call the raw cards that we have to accommodate. We get models of the host controller from the vendor, but, to protect their IP, these models are usually not very detailed, so we have to elaborate the model ourselves. On the DRAM side we have very detailed models. The channel between our chips and host controller crosses the raw card, the connector, and the motherboard. The channel design is controlled by the server manufacturer and it varies from system to system. We use S-parameter models to model a wide range of channel conigurations.

Your Challenges

What technical and business challenges do you face now and in the near future?

As memory speed and density increases, and you want to increase the number of slots per channel, signal integrity is the biggest technical challenge. We have to meet system performance – usually measured by the eye diagram opening – even under the tight constraint of low cost components and material. We’re still using the low cost connectors from the DDR1 days, when frequencies were much lower. We don’t have the luxury of exotic board materials like Duroid or Rogers. We can only use FR4, a higher-end FR4 maybe, but still basically FR4. So, the channel is impaired with HF attenuation, impedance variation, relections, and ISI. Terminations are critical. We don’t have the luxury of differential signaling either: DDR3 is single-ended. In these densely packed circuits, crosstalk is a big issue. Speeds are increasing from 1.6 Gbps/pin in DDR3 to 1.86, and 2.13 gigs in DDR3+ and 3.2 Gbps/pin in DDR4.

Our broad business challenges are time to market and the need to meet design and unit cost targets.

Your Solution

How do you use ADS to solve these challenges?

We have used ADS for ive or six years on several generations of products. The tool helps us evaluate and analyze various channel scenarios and allows us to identify and modify critical design parameters. We just completed one recently on stub resistances. We can explore the design space see the effect on the link-level metrics, such as the eye opening relative to the mask on the eye diagram. It gives us insight into which parameter is most critical and shows what range of values is suitable for the best eye opening. We get increased accuracy by measuring our current high-speed driver and feeding the S-parameters back into the tool to reine the model accuracy for the next generation. Having the two links gives great lexibility because engineers who work mainly in CadenceVirtuoso can access the Keysight simulator, and those who work mainly in ADS can access the Cadence netlist via Dynamic Link.

How does the Advanced Design System help you, and how does it compare to other tools you’ve used?

We have used many different simulation tools and ind that ADS has unique advantages. It is the only tool we have used simultaneously for device modeling to more than 100 GHz, multi-chip designs for telecom ICs, and system analysis for computer memory modules. Its library of components is extensive and vetted by years of experience in the MMIC world – but unlike specialized RF/microwave tools, ADS has the environment that allows us to simulate mixed-signal ICs in time and frequency domains so we can trust the results at any data rate. We have had many experiences where a traditional SPICE tool was used in the distributed-circuit arena and produced nonphysical results – ones that raise more questions than the simulation was intended to solve – and we turned to ADS to resolve the issue.

Your Results:

Can you share any measurable beneits compared to alternate solutions?

We selected ADS because its accuracy saves us re-spins. For example, we’re shipping the existing DDR2 family in high volume – millions of units per month of product – so you can see why any delay due to re-spins is very costly. The cost of a re-spin can be hundreds of thousands of dollars, but the opportunity cost of the delay – ive to six weeks or more – is even more painful in terms of lost revenue–millions of dollars.

×

Please have a salesperson contact me.

*Indicates required field

Preferred method of communication? *Required Field
Preferred method of communication? Change email?
Preferred method of communication?

By clicking the button, you are providing Keysight with your personal data. See the Keysight Privacy Statement for information on how we use this data.

Thank you.

A sales representative will contact you soon.

Column Control DTX