IO Libraries Suite: How do I fix this error message?
IO Libraries Revisions: All Revisions
The following errors are addressed in this document:
- Error 1935 and Error 1603
- Error 1920
- IProcXXX.exe or IO Control could not start error
- KeysightGpib32RenamerService / AgGpib32Controller.exe / AgGpib32Svc.sys error
- Missing or Damaged GPIB-32.dll error in NI-MAX
Error 1935 and Error 1603
Affected versions: All
These are pretty generic installation errors, so there are several possible fixes (do Steps 1 through 4 in order, trying to install the software after each step):
- Disable all Antivirus / Antispyware / Antimalware software while installing the IO Libraries Suite. Programs that monitor for registry changes may also need to be disabled. Remember to re-enable your Security software after the installation is complete.
- Shutdown the Windows Installer Service, then reboot the PC. To shutdown the Windows Installer Service: open the 'Services' item in the Windows Control Panel, select the entry titled 'Windows Installer Service', and click 'Stop'.
- Follow the instructions provided by Installshield for Error 1603: Fatal Error During Installation
- Repair / reinstall the Windows Installer service
Error 1920
Affected versions: IO Libraries Suite 15.0
Some customers see Error 1920 on installation. If you see this problem, install Keysight IO Libraries Suite 15.0 LXI compliant Update (or later). You can download the latest release of the Keysight IO Libraries Suite at www.keysight.com/find/iosuite
IProcXXX.exe or IO Control could not start error
Affected versions: Keysight IO Libraries Suite 15.0 and Keysight IO Libraries Suite 15.0 Patch1
After rebooting your PC, you will get a dialog box that states that IProcXXX.exe or IO Control could not start. This causes intermittent or total failure of instrument I/O communication. Install Keysight IO Libraries Suite 15.0 LXI compliant Update (or later) to fix this problem. You can download the latest release of the Keysight IO Libraries Suite at www.keysight.com/find/iosuite
KeysightGpib32RenamerService / AgGpib32Controller.exe / AgGpib32Svc.sys error
Affected versions: Keysight IO Libraries Suite 14.1
This error has several manifestations, but will mention one of the following items: KeysightGpib32RenamerService, AgGpib32Controller.exe, or AgGpib32Svc.sys. Install Keysight IO Libraries Suite 14.2 (or later) to fix this problem. You can download the latest release of the Keysight IO Libraries Suite at www.keysight.com/find/iosuite
Missing or Damaged GPIB-32.dll error in NI-MAX
Affected versions: NI-488.2 version 2.4 and earlier, Keysight IO Libraries Suite 14.1 and later
If Keysight 488 is enabled in Keysight Connection Expert, you may see the error "Missing or Damaged GPIB-32.dll" when viewing or modifying GPIB properties in NI-MAX (National Instruments Measurement and Automation Explorer). To fix this problem, install NI-488.2 version 2.5 (or later). You can find the latest NI software at www.ni.com
Last Updated: 12June, 2008