Can the 4287A perform calibration for all the "measurement point setup tables" at once?
In manual operation using the front panel keys (or menus) of the 4287A, the calibration for all measurement point setup tables can be performed when "Calibrate all tables" is selected in the Calibration Dialog/Calibration Wizard Setting. However, when a GPIB remote control system is used, you cannot perform the same. The 4287A GPIB commands do not support the calibration for all measurement point setup tables.