Starting Download..
save Save

What is the primary application of the DC resistance measurement function of the 4287A?

The DC resistance measurement function is used primarily for contact check. It checks contact failure between a DUT and the measurement electrodes of an automatic component handler.
Note: Since the DC resistance measurement function is not for accurately measuring the DC resistance of inductive DUTs, the measurement range and accuracy are not as good as dedicated resistance meters.

Was this helpful?


Didn't find what you're looking for?