How do I transfer the current Signal List in my E7400A EMC Analyzer to my PC using remote commands?
There are no remote commands to directly transfer the current signal list to a PC, however, this can be done very easily by first saving the list to a file inside the instrument and then transfer the file.
There are two remote commads that you will need to do this, which are:
-
:MMEMory:STORe:SIGNallist
'filename' -
:MMEMory:DATA?
'filename'
For more information on the use of these commands please see the E7400A Programmer's Guide.
The example VEE program below that uses these commands can be downloaded. This program will show you how you can use these commands to save and transfer the current signal list to your PC.
If you do not have a copy of VEE you can download a trial version from:
If you are using a programming environment other than VEE you can view the attached image file that illustrates how these commands are used.