How can I check for the computer viruses on the ENA?
(SUPPORTED MODELS IN BOLD: E5071C E5072A E5070B/71B E5070A/71A E5061A/62A E5061B E5063A E5091A E5092A)
It depends on the model.
[E5071C, E5072A, E5061B]
Use of an antivirus program is strongly recommended. Obviously Symantec AntiVirus program works well on the ENA. Other antivirus programs should also work well, but not confirmed by Keysight.
[E5070B/71B, E5070A/71A, E5061A/62A]
Enable access to the hard disk drive (HDD) of the ENA from an external PC, and then scan the HDD with anti-virus software installed on the PC. Please refer to the user's guide for enabling the access to the HDD from the external PC.