What accessories should I order with the 8161xA Optical Return Loss Modules?
The following accessories are recommended for use with the 8161xA Optical Return Loss Modules. Please note that the input and the output on the 8161XA Return Loss Modules are angle polished.
- A mainframe
- A calibrated reference reflector
- A DIN connector interface for the reference reflector
- Two (2) connector interfaces for angle polished connectors connector DIN 47256/4108
- The current mainframes are the 8163, 8164 and 8166 mainframes
- The current reference reflector offered by Keysight Technologies is the 81610CC Reference Reflector with DIN connector
-
The model number for the DIN connector interface is the 81000SI
Note: You need an interface connector for use with an angled output ferrules.