Starting Download..
save Save

How do I upgrade my N9010A EXA Signal Analyzer?

Most all of the N9010A options that are sold at the time of instrument purchase are also available as an upgrade option. The upgrade option details can be found in the upgrade tables below.  It is advisable that you view each row for the upgrade of interest, select and read any linked items and view the installation note details before purchasing and installing the upgrade.  In many cases a license key will be required to activate the internal hardware upgrades.  The license certificate and web access is required to redeem a license key.  The upgrade sections are divided into three categories as follows:

  • Internal Hardware Upgrades (Ex. Internal Preamplifier or Fine Step Attenuator)
  • External Hardware Upgrades (Ex. Rackmount Kits or Hard Transit Case)
  • Instrument Software (Ex. Instrument Software or Measurement Application links)

Internal Hardware Upgrades:

Before a hardware upgrade is purchased the following steps should be taken:

  1. View the installation notes by selecting the "Available" links in the tables below for the desired upgrade option.
  2. Determine from the installation note the complexity of the installation and whether you will perform the upgrade yourself or have a Keysight Service Center do it for you.
  3. Review the Utilities, Adjustments & Performance Verification Tests section of the installation note to see what the required adjustments and performance tests are once the upgrade is installed.
  4. Review the following lists of test equipment requirements for each required adjustment and performance test to further determine whether you have the ability to perform the upgrade yourself or have a Keysight Service Center do it for you.

If an upgrade option is going to be installed by an Keysight Service Center, additional labor charges will apply. Your Keysight field engineer can provide an all inclusive quote for this.

All instrument adjustments are automated and require the use of the Keysight Performance Verification & Adjustment Software.

Many hardware upgrades will require the redemption and installation of a license key file to activate the option. Once a redemption certificate is received the license key file can be redeemed at the Keysight Software License Redemption Website

N9010A Internal Hardware Option Upgrades

OptionDescriptionOrder AseDeliveryInstallation NoteUpgrade ContentMinimum FirmwareAdjustments Required1Additional RequirementsIncompatible WithInstalled ByInstallation Time
507
513
526
532
544
Frequency Range Upgrades
 

Refer to table

NoNot Available

Hardware, License Key

Note:
Does not include internal preamplifier upgrade unless frequency range is being upgraded from 32 GHz to 44 GHz

A.10.53Included in upgrade priceRefer to tableNot applicableService Center onlyIncluded in upgrade price
B25Analysis Bandwidth Upgrade, 10 MHz to 25 MHzN9010AK-B25YesAvailableLicense KeyA.01.70NoNoneNoneService Center Recommended4

Install=0.5 Hrs
Adjust & Verify=0.5 Hrs

B403

Important Analysis BW Upgrade Link:

Analysis Bandwidth Upgrade, 10 MHz to 40 MHz, (analyzers with DP2 and/or MPB)N9010AK-B40YesAvailableLicense KeyA.07.00Yes

Yes

NoneService Center Recommended4

Install=0.5 Hrs
Adjust & Verify=0.5 Hrs

Analysis Bandwidth Upgrade, 25 MHz to 40 MHz, (analyzers with DP2 and/or MPB)
 
N9010AK-BU13YesAvailableLicense KeyA.07.00YesYesB40Service Center Recommended4Install=0.5 Hrs
Adjust & Verify=0.5 Hrs
 
Analysis Bandwidth Upgrade to 40 MHz, for Options 507, 513, 526, serial prefix less than MY/SG/US5648 (Includes option MPB)N9010AK-HL4NoAvailableHardware, License KeyA.07.00YesNone

B40, DP2, MPB, 503, 532, 544

Service Center RecommendedInstall=3.0 Hrs
Adjust & Verify=9.0 Hrs
Analysis Bandwidth Upgrade to 40 MHz, for Options 532 & 544, serial prefix less than MY/SG/US5648 (Includes option MPB)N9010AK-HL72No AvailableHardware, License Key A.12.01 Yes Yes

B40, DP2, MPB, 503, 507, 513, 526Service Center Recommended Install=2.0 Hrs
Adjust & Verify=9.0 Hrs
 
Analysis Bandwidth Upgrade to 40 MHz, for Option 503, serial prefix less than MY/SG/US5648N9010AK-HL82No Available Hardware, License Key A.10.53YesYes

B40, DP2, MPB, 507, 513, 526, 532, 544Service Center RecommendedInstall=2.5 Hrs
Adjust & Verify=7.0 Hrs
 
Analysis Bandwidth Upgrade to 40 MHz, for Option 503, serial prefix ≥MY/SG/US5648N9010AK-HL9NoAvailableHardware, License Key A.18.05 Yes Yes

B40, DP2, MPB, 507, 513, 526, 532, 544Service Center RecommendedInstall=2.0 Hrs
Adjust & Verify=7.0 Hrs 
Analysis Bandwidth Upgrade to 40 MHz, for Options 507, 513, 526, serial prefix ≥MY/SG/US5648 (Includes option MPB)N9010AK-HLANoAvailableHardware, License Key  A.18.05Yes Yes

B40, DP2, MPB, 503, 532, 544 Service Center RecommendedInstall=3.0 Hrs
Adjust & Verify=9.0 Hrs 
Analysis Bandwidth Upgrade to 40 MHz, for Options 532 & 544, serial prefix ≥MY/SG/US5648 (Includes option MPB)N9010AK-HLFNoAvailableHardware, License Key  A.18.05 Yes Yes

B40, DP2, MPB, 507, 513, 526 Service Center RecommendedInstall=3.0 Hrs
Adjust & Verify=9.0 Hrs 
CR3Connector Rear, 2nd IF OutputN9010AK-CR3
Pricing
YesAvailableLicense KeyA.07.00NoYes

NoneAdvanced User4

Install=0.5 Hrs
Adjust & Verify=0.5 Hrs

Connector Rear, 2nd I.F. and Arbitrary I.F. OutputsN9010AK-HL3
Pricing
NoAvailableHardware, License KeyA.07.00YesNone

B40, DP2, MPB, 532, 544

MUST READ

Service Center RecommendedInstall=2.0 Hrs
Adjust & Verify=8.0 Hrs
CRPConnector Rear, Arbitrary IF OutputRefer to FAQn/an/an/an/an/an/an/an/a

n/a

Connector Rear, 2nd I.F. and Arbitrary I.F. OutputsN9010AK-HL3NoAvailableHardware, License KeyA.10.05 (Supports N9020-60172 Front End Controller)YesNone

B40, DP2, MPB, 532, 544

MUST READ

Service Center RecommendedInstall=2.0 Hrs
Adjust & Verify=8.0 Hrs
DP2Digital Processor with 2 GB Capture Memory

Only available with original instrument purchase

Note: See option B40 for upgrades (all option B40 upgrades include DP2)

Not applicableNot applicableNot applicableA.07.00NoNot applicableNot applicableNot applicableNot applicable
EA3Electronic Attenuator, 9 kHz to 3.6 GHzN9010AK-EA3YesAvailableLicense KeyA.01.21YesNoneNoneService Center Recommended4

Install=0.5 Hrs
Adjust & Verify=3.0 Hrs

EDPEnhanced Display PackageN9010AK-EDPYesAvailableLicense KeyA.07.00NoNoneNoneUser

Install=0.5 Hrs
Adjust & Verify=0.0 Hrs

EMCBasic EMC FunctionalityN9010AK-EMCYesAvailableLicense KeyA.02.00NoNoneNoneUser

Install=1.0 Hrs
Adjust & Verify=0.0 Hrs

ESCExternal Source Control FeatureN9010AK-ESCYesAvailableLicense KeyA.06.05NoNoneNoneUser

Install=0.5 Hrs
Adjust & Verify=0.0 Hrs

EXMExternal MixingN9010AK-EXMNoAvailableHardware,
License Key
A.10.52Yes532 or 544503, 507, 513, 526Service Center Recommended

Install=1.0 Hrs
Adjust & Verify=1.5 Hrs

FP2Fast Power, up to 40 MHz BWN9010AK-FP2YesAvailableLicense KeyA.14.04NoB40B25 or Std. 10 MHz Analysis BWUserInstall=0.5 Hrs
Adjust & Verify=0.0 Hrs
FSAFine Resolution Step AttenuatorN9010AK-FSAYesAvailableLicense KeyA.01.21YesNoneNoneService Center Recommended4

Install=0.5 Hrs
Adjust & Verify=3.0 Hrs

FS1Fast Sweep Capability ImprovementsN9010AK-R2CYesAvailableLicense KeyA.13.06 NoB40 or DP2 or MPBNoneUserInstall=0.5 Hrs
Adjust & Verify=0.0 Hrs 
FS2Enhanced Fast sweep SpeedN9010AK-FS2YesAvailableLicense KeyA.18.24NoneWindows 7 and DP2Windows XPUserInstall=0.5 Hrs
Adjust & Verify=0.0 Hrs
HDDNo Longer Available, replaced by option SSD (see below)Not applicable Not applicableNot applicableNot applicableNot applicableNot applicableNot applicableNot applicableNot applicableNot applicable
MPBMPB Microwave Preselector Bypass (Requires B40 and/or DP2)N9010AK-MPBNoAvailableLicense KeyA.07.00YesDP2 and/or B40 must be currently installed503Service Center Recommended4

Install=2.5 Hrs
Adjust & Verify=8.0 Hrs

MTUUpgrade to multi-touch user interface when PC6 or PC7 is currently installed; serial prefix >= MY/SG/US5648
 
N9010AK-MTU
 
NoAvailableHardware, License KeyN.ANoN9010A-PC6 or N9010A-PC7 and Serial Prefix >= MY/SG/US5648
 
PC1, PC2, PC3, PC4 or PC5
 
Service Center only "Install=2.5 Hrs
Adjust & Verify = 7.0 Hrs"
 
MTP 

Upgrade to multi-touch user interface; includes PC7 CPU; serial prefix >= MY/SG/US5648  

 N9010AK-MTP No AvailableHardware, License KeyN.ANo Serial Prefix >= MY/SG/US5648

 
PC6 or PC7Service Center only"Install=2.5 Hrs
Adjust & Verify = 7.0 Hrs"
 
NFENoise Floor ExtensionN9010AK-NFEYesAvailableLicense KeyA.14.05NoNoneNoneUserInstall=0.5 Hrs
Adjust & Verify=1.0 Hrs
P03Preamplifier (specified range 100 kHz to 3.6 GHz)N9010AK-P03
 
YesAvailableLicense KeyA.01.21YesNoneNoneService Center Recommended4

Install=0.5 Hrs
Adjust & Verify=2.5 Hrs

P07Preamplifier, 7 GHzN9010AK-P07YesAvailableLicense KeyA.07.00YesNone503Service Center Recommended4

Install=0.5 Hrs
Adjust & Verify=2.5 Hrs

P13Preamplifier, 100 kHz to 13.6 GHzN9010AK-P13YesAvailableLicense KeyA.12.13Yes513, 526, 532, or 544503, 508Service Center Recommended4Install=0.5 Hrs
Adjust & Verify=2.5 Hrs
P26Preamplifier, 100 kHz to 26.5 GHzN9010AK-P26YesAvailableLicense KeyA.12.13Yes526, 532, or 544503, 508, 513Service Center Recommended4Install=0.5 Hrs
Adjust & Verify=2.5 Hrs
P32Preamplifier, 32 GHz (Use with Option 532 only)N9010AK-P32YesAvailableLicense KeyA.10.52Yes532503, 507, 513, 526, 544Service Center Recommended4

Install=0.5 Hrs
Adjust & Verify=3.5 Hrs

P44Preamplifier, 44 GHz (Use with Option 544 only)N9010AK-P44YesAvailableLicense KeyA.10.52Yes544503, 507, 513, 526, 532Service Center Recommended4

Install=0.5 Hrs
Adjust & Verify=3.5 Hrs

PC6

Quad-Core High Performance Processor & Windows Embedded Standard 7 Solid State Drive N9094AK-PC6 & N9094AK-W7X (Under the N9010AK)NoAvailableHardware,
Software,
License Key
A.16.04No2NoneNoneAdvanced UserInstall=0.5 Hrs
Adjust & Verify=0.5 Hrs
CPU/SSD assembly with on-board calibration data memory
PC6SN9094AK-PS6 and N9094AK-W10
(order under N9010AK)
 
No

Available

Hardware

A.25.08
Firmware pre-installed on SSD

No
(if existing cal data can be backed up)

See Install Note link

None


SSD includes Win 10

Windows 7Service Center RecommendedInstall=1.0 Hrs
Adjust & Verify=0.0 Hrs
 
PFRPrecision Frequency ReferenceN9010AK-PFRYesAvailableLicense KeyA.01.21YesNoneNoneService Center Recommended4

Install=0.5 Hrs
Adjust & Verify=1.0 Hrs

R2CRevision to Current, Core Instrument Software Enhancements

N9010AK-R2C

Information on what R2C provides

YesAvailableLicense KeyA.04.25NoNoneNoneUser

Install=0.5 Hrs
Adjust & Verify=0.0 Hrs

SF1Security Features, Exclude Launching ProgramsN9010AK-SF1YesAvailableLicense KeyA.12.09NoNoneNoneUserInstall=0.5 Hrs
Adjust & Verify=0.0 Hrs
 
SF2Security Features, Prohibit Saving ResultsN9010AK-SF1NoAvailableLicense KeyA.14.04NoWindows® 7 Operating SystemNoneUserInstall=0.5 Hrs
Adjust & Verify=0.0 Hrs
 
SSD
 
Windows Embedded Standard 10 Solid State Drive  N9094AK-SSD & N9094AK-W10 (Under the N9010AK) No Available Hardware, Software
 
 A.20.15 No2 PC6 or PC7 PC2, PC4 Advanced User Install=0.5 Hrs
Adjust & Verify=0.5 Hrs
Windows Embedded Standard 7 Solid State Drive N9094AK-SSD & N9094AK-W7X (Under the N9010AK)NoAvailableHardware,
Software,
License Key
A.12.00No2PC4 or PC5PC1, PC2 or PC3Advanced UserInstall=0.5 Hrs
Adjust & Verify=0.5 Hrs
Windows XP For Embedded Systems Solid State Drive Windows XP No Longer AvailableNoAvailableHardware,
Software
NoneNo2PC2, PC3, PC4 or PC5PC1Advanced UserInstall=0.5 Hrs
Adjust & Verify=0.5 Hrs
TDSTime Domain ScanN9010AK-TDSYesAvailableLicense KeyA.14.54No
  1. Windows 7 or Windows 10 OS
  2. N6141A or N6141EMOD EMI Measurement Application
  3. MPB or DP2 or B40
Windows XPUserInstall=0.5 Hrs.
Adjust & Verify=0.0 Hrs.
W10Windows 10 Solid State Drive & Dual Core High Performance Processor N9094AK-PC6 & N9094AK-W10 (Under the N9010AK)NoAvailableHardware, Software, License KeyNoneNo2NonePC6Advanced UserInstall=1.0 Hr
Adjust & Verify=0.0 Hrs
 
Windows 10 Solid State Drive N9094AK-SSD & N9094AK-W10 (Under the N9010AK)NoAvailableHardware, SoftwareNoneNo2PC6, PC7PC1, PC2, PC3, PC4, PC5Advanced UserInstall=1.0 Hrs
Adjust & Verify=0.0 Hrs
 

W7X

Windows Embedded Standard 7 Solid State Drive & Dual-Core High Performance Processor N9094AK-PC4 & N9094AK-W7X (Under the N9010AK)NoAvailableHardware,
Software,
License Key
A.12.00No2NoneNoneAdvanced UserInstall=0.5 Hrs
Adjust & Verify=0.5 Hrs
Windows Embedded Standard 7 Solid State Drive N9094AK-SSD & N9094AK-W7X (Under the N9010AK)NoAvailableHardware,
Software,
License Key
A.12.00No2PC4 or PC5PC1, PC2 or PC3Advanced UserInstall=0.5 Hrs
Adjust & Verify=0.5 Hrs
YASY-Axis OutputN9010AK-YASYesAvailableLicense KeyA.07.00NoNoneNoneAdvanced User4Install=0.5 Hrs
Adjust & Verify=0.5 Hrs


1 While the completion of the recommended adjustments and performance tests for a given option upgrade does verify the functionality of the option, it does not guarantee that the entire instrument meets all published specifications. A full instrument calibration is the only way to guarantee that all instrument specifications are being met
2 The instrument calibration data file MUST be transferred in order for the analyzer to meet specifications. If the cal file is not transferred all adjustments and performance tests must be performed. Refer to the Installation Note for details
3 If MIMO or Single Acquisition Combined Measurements (-XFP options) are being performed, contact your local Keysight representative before upgrading
4 Upgrade can be performed by the User without any performance verification required if the instrument being upgraded is still within it's original factory calibration cycle and no major repairs or adjustments have been performed on it. See the upgrade installation note for more details.
 

N9010A External Hardware Option Upgrades

OptionDescriptionOrder AseDeliveryInstallation NoteUpgrade ContentsMinimum FirmwareAdjustments Required1Additional RequirementsIncompatible WithInstalled ByInstallation Time
1CMRack Mount Kit (Rack Flanges Only)N9010AK-1CM or 1CM013ANoAvailableHardwareNoneNoneNonePRCUserInstall=0.5 Hrs
1CNFront Handle Kit (Handles Only)N9010AK-1CN
or 1CN003A
NoAvailableHardwareNoneNoneNonePRCUserInstall=0.5 Hrs
1CPRackmount Kit w/ HandlesN9010AK-1CP
or 1CP005A
NoAvailableHardwareNoneNoneNonePRCUserInstall=0.5 Hrs
1CRRack Slide Kit (Rack Slides Only)N9010AK-1CR
or E4406-60115
NoAvailableHardwareNoneNoneNonePRCUserInstall=1.0 Hrs
 
DVRUSB DVD-ROM/CD-R/RW DriveN9010AK-DVR
 
NoNoneHardwareNoneNoneNoneNoneNot applicableNot applicable
HTCHard Transit CaseN9010AK-HTC
or E4410-80120
NoAvailableHardwareNoneNoneNoneNoneNot applicableNot applicable
KYBUSB KeyboardN9010AK-KYBNoNoneHardwareNoneNoneNoneNoneNot applicableNot applicable
MLPMinimum Loss Pad, 50Ω Type-N(m) to 75Ω BNC(f)N9010AK-MLP
or 0955-1020
NoNoneHardwareNoneNoneNoneNoneNot applicableNot applicable
MSEUSB MouseN9010AK-MSE
or 0960-2670
NoNoneHardwareNoneNoneNoneNoneNot applicableNot applicable
PRCPortable Configuration

N9010AK-PRC
or N9020-60010

NoAvailableHardwareNoneNoneNone1CM, 1CP, 1CN, 1CRUserInstall=1.0 Hrs

Instrument Software

Instrument Software Update

The software update package for the X-Series Signal Analyzers contains the spectrum analyzer measurement application, all the advanced measurement application software, and all other updates required by the individual measurement assemblies inside the instrument.

Keysight recommends updating the instrument software version whenever an internal hardware upgrade or measurement application is installed into the analyzer.

The latest revision of the instrument software installer can be found at:

Measurement Applications:

To see the complete list of software measurement applications available for the N9020A Signal Analyzer see:

Measurement Applications require the redemption and installation of a license key file (.lic). Measurement application upgrades are meant to be performed by the customer, and no adjustments or performance verification tests are required.

In order to redeem a license key, the end user must have a valid redemption certificate and then go to the Keysight Software License Redemption Website

Available Accessories:









































Was this helpful?


Didn't find what you're looking for?