Do I need to order option 054 (High Speed Test Extensions) for the N6751A, N6752A, and N6754A High Performance DC Power Modules, when I plan on usi...
Option 054 is not required when the DC Power Module will be used in a DC Power Analyzer. The scope, arbitrary waveform generator, and the datalogger are all part of the functionality of the DC Power Analyzer. Option 054 is required to use the lists and digitizer functionalities in the N6700B, N6701A, and N6702A Low-Profile Modular Power System Mainframes.