By Topic

By Industry/Technology

By Type of Content

By Product Category

76-100 of 1163

Sort:
Is "offset compensation" available for resistance measurements with the 34405A Digital Multimeter?
No, "offset compensation" is not available for resistance measurements with the 34405A Digital Multimeter….

FAQ 2013-11-15

What are the conditions that will cause the U1270 series handheld multimeter to display Incorrect DC Voltage values at DC measurement mode when signal
The error value may occur if the Filter is not enabled...

FAQ 2013-11-10

Which version of the CPRI standard is the N5120A compliant to?
The N5120A is compliant up to v1.1.

FAQ 2013-09-27

Why is the segmented memory acquisition mode useful and which Infiniium oscilloscopes support it?
Segmented memory mode offers more efficient acquisition memory usage for storing waveforms with events of interest that are separated by long periods of time. All currently shipping Infiniiums and many older units support segmented memory.

FAQ 2013-09-18

How can I source a pulsed signal on the B2961A/B2962A?
Click the above link for details.

FAQ 2013-09-16

I am looking at a 160 MHz OFDM signal at 5 GHz on my MXA or PXA signal analyzer. Why can’t I see the whole signal?
The instrument preselector is limiting the bandwidth of the MXA or PXA input.

FAQ 2013-08-07

Can I use the MXA or PXA real-time Frequency Mask Trigger (FMT) to provide a trigger output that can be used to trigger another device?
Yes, you can configure the MXA or PXA to provide a trigger output when using FMT.

FAQ 2013-08-07

Can I get the real-time I/Q samples out via LAN on my MXA or PXA signal analyzer with option RT1 or RT2?
No, however you can save the real-time trace (Frequency & Amplitude) data into a .csv file from the spectrogram trace (10,000) traces.

FAQ 2013-08-07

How do you clear the M9381A PXIe Vector Signal Generator and M9380A PXIe CW Source modules memories?
Please refer to the documents for a comprehensive listing of memory installed into these products.

FAQ 2013-08-06

Replacement of Control XTP, Module Control Card
Frequently Asked Questions about XTPA Module Control Card

FAQ 2013-06-11

Is it possible to adjust the phase offset using degrees instead of radians?
Yes. Select View -> Customize Pattern Item Table and toggle the ‘phase offset in degrees’ button

FAQ 2013-05-16

Are there any options to adjust the pulse definitions within Signal Studio for pulse building?
No, at the moment the rise and fall times are defined by their 0-100 percent points and the pulse width is defined to be the 100-100 percent point.

FAQ 2013-05-16

Is there a way to put insert a missing pulse into the signal?
Yes, you can add a “Off time” object to the pulse pattern and change the duration to meet your pulse requirements.

FAQ 2013-05-16

How to add N9051A, Pulse Measurement Software, to the mode key selections.
X-Series signal analyzer with Windows 7 and Software versoin A.12.xx installed may not list N9051A as selection avilable under the Mode key.

FAQ 2013-05-16

How do I change the 10 MHz reference source if Signal Studio for pulse building doesn’t detect the reference?
Most of the time, Signal Studio will recognize the reference; however, it can be changed in the download -> customize menu.

FAQ 2013-05-16

Does the ENA 6 series have the swept sweep mode in the frequency sweep?
No. The E5061A/62A and E5061B have only stepped sweep mode in the frequency sweep.

FAQ 2013-04-25

How do you clear the M9536A Embedded Controller memories?
Please refer to the link below for the procedure on how to clear the memories for the M9536A Embedded Controller.

FAQ 2013-04-01

How do you clear the M9036A Embedded Controller memories?
Please refer to the link below for the procedure on how to clear the memories for the M9036A Embedded Controller.

FAQ 2013-04-01

What USB storage devices are compatible with the MXG?
The MXG is now compatible with most USB storage devices.

FAQ 2013-03-13

Is it possible to convert configuration files from the older 1670- and 16700-series Keysight logic analyzers to the new 16800/1690/16900-series anal...
Yes. The Keysight Logic Analyzer application for 1680/90/800/900-series logic analyzers includes utilities for translating configuration files from 167xG and 16700-series logic analyzers.

FAQ 2013-03-13

Do User channel corrections cover multiple attenuator steps?
Yes. Bypass step, 0 dB step, and 5 dB step.

FAQ 2013-02-26

Sample “testplan” for Utility card & FR3070A
Sample “testplan” for Utility card & FR3070A from manufacturing site

FAQ 2013-02-18

When I use the 30-day trial license of the Signal Studio for WiMAX™, how can I check the number of days remaining on temporary license?
Press the front panel keys: Utility > Instrument Adjustments > Instrument Options > Waveform Licenses

FAQ 2013-01-28

66xxA, E363xA and E364xA: Ca Keysight Power Supplies Sink Current?
Yes! Sinking, or down-programming, is the ability to pull current into the positive terminal of a power supply.

FAQ 2013-01-22

When would I use ALC Hold?
ALC Hold is used for pulses with rise and fall times greater than 100 ns. It is used with pulses that do not have constant envelope modulation (such as AM Step), and with multiple pulses where the pulses have different amplitudes.

FAQ 2012-12-30

Previous 1 2 3 4 5 6 7 8 9 10 ... Next