이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

상세 분류

상세분류 제거

산업/기술

분야별 검색결과

76-100 / 745

정렬방식:
Principal Component Analysis-Based Compensation for Measurement Errors
This paper examines some issues and trends that justify adding features to IEEE 1149.1 that will facilitate safe, fast and effective initialization of a board or system, to get it ready for testing. Published with kind permission of the IEEE

기사 2015-06-08

PDF PDF 1.86 MB
Faster Testing with High-Performance Spectrum Analysis in a VNA - Article Reprint
Article reprint from the June 2015 issue of Microwave Journal highlighting the new spectrum analyzer option for the PNA Series.

기사 2015-06-01

PDF PDF 1.23 MB
The key to early 5G investigation – test tools for new network paradigms
Electronic Products and Technology, May 2015 article discusses the needs of 5G, areas of investigations and available test tools to make it happen

기사 2015-05-19

Thales Nederland Reaps the Benefits of Keysight Onsite Calibration - Case Study
Thales Nederland experienced product shipment delays and cost overruns due to long turn around times for calibration. Keysight solved their challenge with the solution of Onsite Calibration.

사례연구 2015-04-21

PDF PDF 50 KB
5G 파형 발생 및 분석을 위해 유연한 Testbed 구현 - 백서 (영어)
이 백서는 성능이 입증된 상용 소프트웨어 및 하드웨어를 포함하고 있는 유연한 5G testbed에 대해 설명하며, 5G 기술의 설계 및 테스트 과제에 대해서도 검토합니다.

기사 2015-04-20

PDF PDF 1.95 MB
Risk factors of Utilizing Unauthorized Third-Part Suppliers for In-Circuit Test - Case Study
This paper describes the potential risks customers may have to face by engaging services from unauthorized 3rd party suppliers for 3070 and i3070 products and services.

사례연구 2015-04-15

PDF PDF 2.02 MB
Improving IBIS-AMI Model Accuracy: Model-to-Model and Model-to-Lab Correlation Case Studies - Articl
This DesignCon 2014 paper presents case studies for model-to-model & model-to-lab correlation methods & compares favorable/unfavorable factors for both methods. 10G, 11.5G and 23G SerDes data are used as examples.

기사 2015-04-02

PDF PDF 3.34 MB
Utilizing Commercial Best Practices for Success in NewSpace - Application Note
NewSpace is driving disruption that we haven’t seen since the original space race in the 1960’s. This paper describes the challenges that the new and unique business models put on electronic design and test strategies and processes. We will present ways to enable much higher volume with much lower cost while maintaining high quality.

기사 2015-03-31

PDF PDF 451 KB
PCI Express Receiver Testing Responds To New Challenges - Article
PCI Express Receiver Testing Responds To New Challenges

기사 2015-03-24

A Nonlinear Model Complier for RF/MICROWAVE Engineers
This Article presents Genesys latest release which includes a powerful Verilog-A compiler technology and hence enhancing the accuracy of simulation.

기사 2015-03-18

PDF PDF 545 KB
AWG M8195A won Lightwave award 2015
The 2015 Lightwave Innovation Award Elite Scores

기사 2015-03-17

University of Leeds Showcases Two Engineering Research Labs

기사 2015-02-11

Signal-Generation Advances Support Electronic Warfare’s Evolution

기사 2015-01-28

University of Utah Goes to Extremes to Investigate the Characteristics of Polar Ice
Read how Professors Ken Golden and Cynthia Furse and colleagues from the University of Utah used Keysight’s FieldFox handheld analyzer to measure the electromagnetic properties of polar ice

기사 2015-01-07

Signal-Generation Advances Support Electronic Warfare’s Evolution

기사 2014-12-31

PDF PDF 564 KB
mmWave MIMO Channel Sounding for 5G: Technical Challenges and Prototype System
In this paper, ww focus on how to setup mmWave MIMO channel sounding system with commercial instruments to fulfill the major technical challenges.

기사 2014-12-18

프로스트 앤 설리번(Frost & Sullivan) 2014 글로벌 계측 소프트웨어 시장 리더십 어워드 – 기사 재인쇄 (영어)

기사 2014-11-14

PDF PDF 1.97 MB
Design of an 8×8 MIMO Broadband RF Subsystem for Future WLAN
Microwave Journal, November 13, 2014 article by Southeast University describes a broadband 8×8 MIMO RF subsystem with large area coverage for next generation WLAN in the 5 GHz band.

저널 2014-11-13

Engineering Students in Brazil Learn with Hands-on Projects
Engineering Students in Brazil Learn with Hands-on Projects

기사 2014-10-28

IRCICA Creates a Telecommunications Test Platform for Industrial and Academic Research
IRCICA Creates a Telecommunications Test Platform for Industrial and Academic Research

기사 2014-10-16

AWG article - MWJ product feature
AWG article - MWJ product feature

기사 2014-10-14

MIT Lives Up to its Motto: Mind and Hand
MIT Lives Up to its Motto: Mind and Hand

기사 2014-09-21

HeatWave Case Studies
HeatWave Electro-Thermal simulation case studies.

사례연구 2014-09-18

HeatWave Technical Papers
Links to various technical papers related to HeatWave Electro-Thermal analysis software.

기사 2014-08-27

Mechanism of Jitter Amplification in Clock Channels
In this paper. jitter amplification in clock channels is analyzed analytically using the techniques developed in "Frequency domain analysis of jitter amplification in clock channels."

기사 2014-08-04

PDF PDF 715 KB

이전 1 2 3 4 5 6 7 8 9 10 ... 다음