您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

技術支援

電子量測

依產品型號搜尋可用的支援:

縮小範圍

移除所有細分

依產業/技術

依內容類型

1-25 / 448

排序:
Customizing Tables Just Got Easier with a New Python Module for MQA Software
Working with data tables is a basic skill every engineer learns early on in their career. When organized properly, tables can summarize a great deal of device data into a helpful information format, and that makes them extremely useful.

專文 2017-07-12

Applying a Very Wide-Bandwidth Millimeter-Wave Testbed to Power Amplifier DPD
5G designs that use wide-bandwidth digital modulation require new test technologies. Our latest 5G whitepaper presents a testbed for generating and analyzing millimeter-wave signals with 8 GHz bandwidth.

專文 2017-06-06

Extending the Power of IC-CAP Software with Python—PyVISA Instrument Control
Learn how to access the full capabilities of PyVISA from IC-CAP 2016 and create transforms for instrument control and data acquisition over any supported interface.

專文 2017-05-31

S-parameters: Signal Integrity Analysis in the Blink of an Eye
This article discusses new concepts for serial link design and analysis as applied to physical layer test and measurement techniques. Novel test fixtures and signal integrity software tools will be discussed in real world applications in the form of design case studies.

專文 2017-05-30

The Melting Trace Paradox
Unlike other famous paradoxes such as the Zeno’s paradox, where Achilles and the Tortoise are involved, the melting trace paradox is one with a segment of copper trace and a current source.

專文 2017-05-24

Early Design Review or Boundary Scan in Enhancing Testability and Optimazation of Test Strategy
With complexities of PCB design scaling and manufacturing processes adopting to environmentally friendly practices raise challenges in ensuring structural quality of PCBs.

專文 2017-05-08

PDF PDF 624 KB
SRAM Cell Model Generation and Modeling Efficiency Take Center Stage in New Software Releases
Accurate and efficient modeling is critical to successful design, especially when it comes to the Static Random Access Memory (SRAM) cell, the minimum geometry devices in integrated circuit technology.

專文 2017-05-04

Villanova Professor and Students “Bang Heads” for Nanotechnology Research
Dr. Gang Feng, Associate Professor in the Department of Mechanical Engineering at Villanova University, is using advanced materials measurement technology to understand concussions, energy storage, and more.

專文 2017-04-21

Expanding IEEE Std 1149.1 Boundary-Scan Architecture Beyond Manufacturing Test of PCBA
This paper will discuss the expanded use of boundary-scan testing beyond the typical manufacturing test to capture structural defects on a components/devices in a Printed Circuit Board Assembly (PCBA)

專文 2017-04-01

PDF PDF 860 KB
Ensuring High Signal Quality in PCIe Gen3 Channels
This Signal Integrity Journal article written by Keysight engineer, Anil Kumar Pandey includes the challenges of maintaining transmission channel signal quality in today's PCIe Gen3 Channels.

專文 2017-03-14

Internet of Things (IoT) Teaching Solution – IoT Systems Design

專文 2017-03-14

Internet of Things (IoT) Teaching Solution – IoT Fundamentals

專文 2017-03-14

Keysight Translator for QDART Test
Keysight Translator software for QDART

專文 2017-03-09

Heidi Barnes: DesignCon 2017 Engineer of the Year
EDN Network's Martin Rowe interviews Heidi Barnes, DesignCon 2017 Engineer of the Year.

專文 2017-02-23

為何需要元件建模服務?
元件建模和特性分析是成功 IC 設計的基礎。

專文 2017-02-03

Addressing The Challenges Facing IoT Adoption - Article Reprint
Addressing The Challenges Facing IoT Adoption - Article Reprint

專文 2017-01-23

PDF PDF 2.25 MB
Keysight One-Stop Calibration Capabilities – Americas
View our capabilities for dimensional / optical; electrical – DC, low frequency; electrical – optical; electrical – RF, microwave, millimeter wave; physical / mechanical

專文 2016-12-15

HUAWEI demonstrates 112 Gb/s PAM-4 optical signal transmission with M8196A AWG
112 Gb/s PAM-4 Optical Signal Transmission over 100-m OM4 Multimode Fiber for High-Capacity Data-Center

專文 2016-12-05

Integrating Multiple Technology Devices onto Laminate-Based Multi-Chip-Modules
Microwave Product Digest (MPD) featured article on "Integrating Multiple Technology Devices onto Laminate-Based Multi-Chip-Modules Using an Integrated Design Flow", written by Keefe Bohanan, Applications Engineer District Manager for Keysight EEsof EDA.

專文 2016-11-29

PDF PDF 3.90 MB
Direct-Synthesis Software Approach Facilitates Filter Design
This Microwaves & RF article discusses how Genesys software can be used to design filters with the direct-synthesis technique. A lowpass filter example is presented to illustrate the software’s capabilities.

專文 2016-11-28

Using DSP and RF circuit co-design to reduce risk and cost
For modern design organizations, it’s now more imperative than ever that they simulate both Digital Signal Processor (DSP) and RF circuits together at the system level using mixed signals.

專文 2016-10-11

Software plus signal generators and analyzers support IEEE 802.11p design and test
Jungik Suh, marketing program manager, Automotive & Energy Solutions, Keysight Technologies, provides input on several Keysight solutions for the connected-car arena for Evaluation Engineering's October print special report on automotive test.

專文 2016-10-05

A Quick Fix for Poor Capacitor, Inductor and DC/DC Impedance Measurements
Modern Test & Measure article by Steve Sandler (Picotest) explains why you need an extended range, partial S2p measurement and how to make this improved measurement.

專文 2016-10-03

Best Practices for Connector Models
Eric Bogatin, Signal Integrity Journal Editor, discusses best practices for connector modeling and measuring with Heidi Barnes, Keysight ADS application engineering specialist, and Jim Nadolny, Principle SI Engineer for Samtec.

專文 2016-09-30

Correlating simulation and measurement for a USB Type-C reference channel (Part 1)
This article from Electronic Products discusses a step-by-step process that signal integrity engineers can follow to ensure their success in designing with USB Type-C devices.

專文 2016-09-21

1 2 3 4 5 6 7 8 9 10 ... 下一頁