By Topic

By Industry/Technology

By Type of Content

By Product Category

1-25 of 1164

Sort:
Can a CalPod system be used with the N1500A software?
No, the CalPod and N1500A Software are not compatible.

FAQ 2016-11-02

Does the Maury Microwave MT7553B03 50 GHz Noise Receiver Module lower the effective noise figure of the N5245A beyond that of option 029?
Yes, the NF of the 50 GHz PNA-X is about 10 dB for most of its range while the typical NF from the MT7553B03 is 6 dB.

FAQ 2016-11-02

Does the noise figure application on the PNA-X (option 029) provide a full noise-parameter system (tuners and software)?
No, we don’t provide a full noise-parameter system. Click on the question for additional information.

FAQ 2016-11-02

34972A with USB data logging may eventually freeze. How to prevent?
Yes, experience has shown that using a powered USB 2.0 Hub between the 34972A and the PC usually eliminates the problem.Using LAN instead of USB is the recommended solution if possible.

FAQ 2016-10-26

Can I determine if a Keysight Signal Generator needs to be operated in terms of a status value or the temperature that it was last performed?
Keysight signal generators do not have any circuitry to monitor temperature values, or even log temperatures, inside any of our signal generators.

FAQ 2016-10-21

How do I create a Mono FM Signal using N5182B MXG ARB?
You can configure N7611B Signal Studio Broadcast Radio to play a mono/FM signal.

FAQ 2016-10-21

How many carriers can the MXG support in Carrier Aggregation mode?
One MXG can support one instance of the Carrier Aggregation mode. One instance of the Carrier Aggregation mode supports 5 component carriers.

FAQ 2016-10-11

For my UXA Signal Analyzer, what applications support option H1G (1 GHz Analysis Bandwidth) and what additional functionality does it provide?
Option H1G also includes the B2X digitizer. Therefore, option H1G is supported by all applications that support B2X up to at least 255 MHz bandwidth. Option H1G additionally provides 1 GHz analysis bandwidth for some other measurement applications.

FAQ 2016-10-07

Is option RTS necessary for streaming with bandwidths greater than 40 MHz?
Option RTS is necessary for streaming bandwidths greater than 40 MHz. Either real-time option, RT1 or RT2, is required. Even though these options are license key enabled, they require the analyzer to have B85, B1X, B2X, or B5X.

FAQ 2016-10-07

Is Option RTS a license key or hardware upgrade?
Option RTS is a hardware and license key upgrade. Therefore, this upgrade requires the analyzer to be returned to Keysight.

FAQ 2016-10-07

Why is Option DP2 or B40 recommended on the spectrum analyzer (EXA, MXA, PXA) with the EMI Measurement Application(N6141A)?
Time Domain Scan (TDS), Monitor Spectrum, and Amplitude Probability Distribution (APD) all require 2 GB of Capture memory (option DP2). Option B40 includes DP2, so having either option B40 or DP2 will work equally as well for N6141A.

FAQ 2016-10-07

FieldFox Manuals, Firmware, Software and Product Support
Manuals, firmware upgrade, software trials & upgrade and support page for FieldFox analyzers

FAQ 2016-09-19

For 89601B, can I purchase more than 1 year of VSA Software Subscription Service?
Yes, you may add multiple quantities of 89601BU-012.

FAQ 2016-07-08

In 89601B, I want to know if the setting is finished. Is there a .NET equivalent of *OPC?
No, there is no equivalent *OPC command since this is typically not required. The command "Measurements.WaitForMeasurementDone" can wait for the end of the measurement.

FAQ 2016-07-08

In N7625B, how many instances of carriers and carrier aggregations do the software support?
One connected signal generator can support one instance of Carrier Aggregation mode. One instance of Carrier Aggregation can support 5 component carriers.

FAQ 2016-07-08

In 89601B Digital Demodulation, how can we perform Pi/4 QPSK?
QPSK can be used for Pi/4 QPSK modulation analysis, but the demodulated bits will not be valid.

FAQ 2016-07-08

Can the U4431A MIPI M-PHY protocol analyzer be controlled from an external PC via the AXIe mainframe's USB port?
Yes, the USB connected chassis option (M9502A-U20/M9505A-U20) is a viable connection strategy when using the U4431A M-PHY Protocol Analyzer instrument.

FAQ 2016-07-08

In 89601B for APSK demodulation, how does the LDPC parameter affect measurements?
LPDC adds bit encoding.

FAQ 2016-07-08

Why isn’t the unit being discovered by VSA software hosted inside the instrument itself?
Check to see if Keysight Technologies is returned from the analyzer as part of the *IDN query.

FAQ 2016-07-08

What termination model (Balanced vs. Unbalanced) should I use for my M8000 BERT?
For M8000 (M8041A/51A/61A/62A) BERT data outputs, a Termination Model must be selected in the Amplifier section of the Parameters window, Balanced or Unbalanced.

FAQ 2016-07-08

In 89601B Vector Mode, what is the maximum Main Time length achieved?
Main Time is limited to 524288 samples.

FAQ 2016-07-08

In VSA software, how can I export data from the coordinate transformed data that is displayed on the trace?
This can be done by copying/pasting data, or via the API.

FAQ 2016-07-08

What is the phase noise sensitivity of the E5052B with E5053A and 11970 Mixers?
Please refer to this document.

FAQ 2016-03-29

What is enhanced overload detection and power trip function?
Since the autumn in 2015, the E5061B Option-115/117/135/137/215/217/235/237 ships with enhanced overload detection and power trip function. The E5061B Option-3L5 does not have this function.

FAQ 2016-01-28

How do I measure accurately below -60dBm using U2040 X-Series Sensor?
Click on the question above for recommended steps.

FAQ 2015-12-14

1 2 3 4 5 6 7 8 9 10 ... Next