Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Electronic Measurement

Support by Product Model Number:

1-12 of 12

Sort:
Are the input channels on the U1602A and U1604A Handheld Oscilloscopes isolated?
No, the scope channels 1 and 2 on the U1602A and U1604A Handheld Oscilloscopes are not isolated. They share the same ground.

FAQ 2013-11-17

Do the handheld spectrum analyzers have a fan or vent?
No, the HSAs have design that is fanless and has no vent.

FAQ 2012-02-20

Can event (trigger) logged data be transferred to the GUI DATA LOGGER?
No, data can only be transferred for manual logged data and interval logged data.

FAQ 2011-05-05

Why am I getting a reading instead of zero when using U1252A/U1253A frequency counter measurement function although no measurement was done…
After the probes are connected to the U1252A/U1253A, the measured value will be automatically zeroed.

FAQ 2010-08-09

How long can the batteries of the U1241B or U1242B Handheld Digital Multimeter last?
The batteries that are supplied with the U1241B or U1242B Handheld Digital Multimeter can last for more than 200 hours under normal use.

FAQ 2010-02-21

Why is the battery life of the U1253B Handheld Digital Multimeter (DMM) typically shorter than the battery life of the U1251B/U1252B?
The battery life of the U1253B Handheld Digital Multimeter (DMM) is typically shorter because its display brightness is set to the highest….

FAQ 2010-02-21

Can I use regular AAA batteries in the U1241B and U1242B Handheld Digital Multimeters?
Yes, you may use regular AAA batteries for the U1241B and U1242B Handheld Digital Multimeters….

FAQ 2010-02-21

What is the recommended battery type for the U1251B, U1252B and U1253B Handheld Digital Multimeters (DMM)?
The recommended battery type for the U1251B, U1252B and U1253B Handheld Digital Multimeters (DMM) are described on the table below……

FAQ 2010-02-21

What is the update rate for U1600A series handheld scope?
update rate is 14 waveforms per second

FAQ 2009-08-06

What is the recommended battery type for the U1251A, U1252A and U1253A Handheld Digital Multimeters (DMM)?
The recommended battery type for the U1251A, U1252A and U1253A Handheld Digital Multimeters (DMM) are described on the table below……

FAQ 2009-06-10

What type of USB cable do the U1602A and U1604A Handheld Oscilloscopes use?
The U1602A and U1604A Handheld Oscilloscopes use the USB type-A to mini-B cable….

FAQ 2009-05-03

Why is the battery life of the U1253A Handheld Digital Multimeter (DMM) typically shorter than the battery life of the U1251A/U1252A?
The battery life of the U1253A Handheld Digital Multimeter (DMM) is typically shorter because its display brightness is set to the highest….

FAQ 2008-10-09