전문가 상담

기술 지원

X-시리즈 신호 발생기 (MXG, EXG)

모델번호로 검색: 예제: 34401A, E4440A

1-25 / 98

정렬방식:
How do I upgrade my N5172B EXG X-Series RF Vector Signal Generator?
Find Information on hardware upgrades, instrument firmware and more.

FAQ 2014-10-14

How do I upgrade my N5193A UXG Agile Signal Generator?
Find Information on Hardware Upgrades, Instrument Software, etc.

FAQ 2014-10-01

Signal Generator Firmware Update Center
Download signal generator firmware, release notes, upgrade guide and FAQs.

FAQ 2014-06-10

X시리즈 신호 발생기의 출력파워가 향상 됐나요?
네, MXG에서 규정된 출력 파워가 +23dBm에서 +24dBm으로 변경 되었습니다.

FAQ 2014-04-28

X시리즈 신호 발생기에서 외부에서 입력 받는 I와 Q신호에 대해 독립적으로 감쇄를 적용할 수 있나요?
네, 가능합니다. 1세대 MXG (N5182A)에서 향상된 특징입니다.

FAQ 2014-04-28

What is Option ALB on the MXG signal generator?
Option ALB on the MXG enables LAN LXI class B compliance. This option is included standard on all new MXG’s shipped since June 2009. MXG’s shipped before June 2009 can be upgraded by ordering option N51xxAK-ALB. Contact Keysight for more details.

FAQ 2014-04-07

How do I upgrade my N5161A MXG ATE Analog Signal Generator?
Find Information on Hardware Upgrades, Instrument Software, etc....

FAQ 2014-04-07

How do I upgrade my N5183A MXG Microwave Analog Signal Generator?
Find Information on Hardware Upgrades, Instrument Software, etc....

FAQ 2014-04-07

How do I upgrade my N5182B MXG X-Series RF Vector Signal Generator?
Find Information on hardware upgrades, instrument firmware and more.

FAQ 2014-04-02

How does the MXG N5182B achieve 160 MHz of bandwidth with a sample rate of 200 MSa/sec?
The MXG and EXG BBG has an arbitrary fractional re-sampling ASIC that will up-sample and interpolate the user sample rate setting from the front panel. For example ...

FAQ 2014-03-12

What is included with Option UK6?
Beginning December 19, 2013, the list below describes what will be included with Option UK6:

FAQ 2014-02-27

How do I upgrade my N5181B MXG X-Series Analog Signal Generator?
Find Information on Hardware Upgrades, Instrument Software, etc....

FAQ 2014-01-24

How do I upgrade my N5171B EXG X-Series Analog Signal Generator?
Find Information on Hardware Upgrades, Instrument Software, etc....

FAQ 2014-01-24

How do I upgrade my N5173B EXG Microwave Analog Signal Generator?
Find Information on Hardware Upgrades, Instrument Software, etc....

FAQ 2014-01-23

How do I upgrade my N5183B MXG Microwave Analog Signal Generator?
Find Information on Hardware Upgrades, Instrument Software, etc....

FAQ 2014-01-23

X-series 신호 발생기에서 펄스 연결 발생(Pulse train Generator)옵션 320을 사용하기 위해서는 옵션 UNU (펄스변조옵션) 또는 UNW (좁은펄스변조옵션)를 필요로 합니까?
네, 옵션 320 (연결 펄스 발생)은 좁은펄스변조 옵션(narrow pulse)인 UNW가 필수 옵션 입니다.

FAQ 2014-01-22

What is the RF Test Blog?
RF engineers know that making good measurements is a challenge. The RF Test Blog was created as a resource for RF engineers to find ways to make better RF measurements.

FAQ 2013-12-17

X-시리즈 신호발생기에서 지원되는 USB 파워 센서는 어떤 것이 있나요?
모든 키사이트의 USB U200xx 파워 센서가 지원되고 있습니다. 향후 키사이트 USB U202xx 피크 파워 센서와 U8481 Thermocouple 파워 센서가 지원될 예정입니다.

FAQ 2013-10-20

What calibrations are available on X-Series, PSA, ESA analyzers and X-Series, ESG-C, PSG Signal Generators at time of initial sale from the factory?
Details regarding time of sale calibrations can be found here...

FAQ 2013-10-15

When should I use Real-time Custom Modulation vs. Arb Custom Moduation vs. Creating my own IQ waveform?
It is always easier to use the real-time custom modulation mode inside the instrument until you run out of the flexibility.

FAQ 2013-08-14

N5181A 업그레이드 표

FAQ 2013-08-05

How do I find the HOST ID of my instrument or PC?
Keysight software options are licensed to many different types of hardware, using a unique hardware identifier called the Host ID. The Host ID is composed of 1, 2, or 3 elements, depending upon the software model and the target hardware platform.

FAQ 2013-05-07

What USB storage devices are compatible with the MXG?
The MXG is now compatible with most USB storage devices.

FAQ 2013-03-13

Is the performance of 0.4% EVM for 160 MHz 802.11ac best test result or average performance for N5182B MXG or N5172B EXG X-Series signal generators?
0.4% EVM is characteristic data of a small sample of N5182B MXG signal generators

FAQ 2013-02-26

Can running user correction calibration over a narrower range improve calibration?
No, the number of points is always fixed at a 5 MHz interval

FAQ 2013-02-26

1 2 3 4 다음