Sprechen Sie mit einem Experten

Technical Support

Spectrum Analyzers (Signal Analyzers)

Find by Product Model Number: Examples: 34401A, E4440A

1-25 of 839

Sort:
Where can I find FieldFox Firmware, Software and Product Support information?
A central FieldFox page that includes links to: Upgrades, Firmware, Data Link software, User's Guides, Programming Guide, Secured environment operation, supported Calibration kits and more.

FAQ 2015-06-23

Does the M9290A CXA-m PXIe signal analyzer offer a tracking generator?
Yes, M9290A CXA-m has optional tracking generator function.

FAQ 2015-06-04

Signal Analyzer IVI and MATLAB Instrument Drivers
Supported models: N9000A, N9010A, N9020A, N9030A, N9038A, E4406A, E4440A, E4443A, E4445A, E4446A, E4448A, N8201A, E4447A, E4401B, E4402B, E4403B, E4404B, E4405B, E4407B, E4408B, E4411B, E7401A, E7402A, E7403A, E7404A, E7405A, M9290A, N9040B, N9038A

FAQ 2015-05-27

Upgrading 89600 VSA Software
Adding new options, upgrading to new revisions, and adding additional applications is described in this document.

FAQ 2015-04-21

Signal & Spectrum Analyzer Benchtop/Handheld Firmware Update Center
To access the most recent version of firmware or software for signal and spectrum analyzer - benchtop and handheld models.

FAQ 2015-04-08

How do I upgrade my PSA Series Spectrum Analyzer?
Find information on Hardware Options, Measurement Personalities, Connectivity Methods, Firmware Upgrades, etc…

FAQ 2015-04-06

Can I measure VSWR, return loss and DTF with my handheld spectrum analyzer?
Yes, the HSA N9342C handheld spectrum analyzer with option CA7 and TG7 support to read VSWR.

FAQ 2015-03-17

Can I use a Windows 7 PC to upgrade my PSA Series Spectrum Analyzer?
In Windows 7 you can use the Windows XP mode to run the PSA Firmware Update Program.

FAQ 2015-03-12

How do I upgrade my N9038A MXE EMI Receiver?
Find Information on Hardware Upgrades, Instrument Software and Measurement Applications, etc...

FAQ 2015-02-27

What are the login and passwords that are used on the X-Series Signal Analyzers?
There are two different login accounts: User account and Administrator account

FAQ 2015-01-13

30-Day Free Trial for X-Series Measurement Applications for X-Series Signal Analyzers
30-day trial license available for the X-Series measurement applications for X-Series signal analyzers.

FAQ 2014-12-19

How do I upgrade my Spectrum / Signal Analyzer?
Information to perform a spectrum analyzer upgrade or signal analyzer upgrade.

FAQ 2014-12-18

What hardware platforms are no longer supported by the 89600 VSA software?
A list of discontinued hardware by version number

FAQ 2014-12-16

What hardware platforms are supported by the 89600 VSA and 89600 WLA Software?
The measurement hardware front ends include supported by the current version of software are listed here.

FAQ 2014-12-16

89600 VSA software and X-Series signal analyzer software compatibility matrix
Supported versions listed here

FAQ 2014-12-16

How do I upgrade my M9290A CXA-m PXIe Signal Analyzer?
Find Information on Hardware Options, Measurement Applications, etc....

FAQ 2014-11-17

How do I find my Host ID when I run software on a PC?
For the PSA model, when requesting an N9051A trial

FAQ 2014-10-31

I ordered the N9051A, but it is no longer installed on the signal analyzer. The N9051B is installed, but my N9051A licenses don’t work. What shou
The N9051B is the recommended replacement for N9051A. The N9051A license can be upgraded by adding a low-cost N9051B-A2B license.

FAQ 2014-10-21

If I have N9051A Pulse Measurement Software, how do I upgrade to N9051B?
Order N9051B Option A2B to receive a user-installed software license, which causes any existing N9051A licenses to be recognized as N9051B licenses. The N9051B-2FP license is required, while all others are optional and independent of each other.

FAQ 2014-10-21

How is the N9051B Pulse Measurement Software delivered, installed and licensed?
Important: N9051B runs only on the CPU inside an X-Series signal analyzer, which must be Windows 7 and 64-bit. See the FAQ for further details.

FAQ 2014-10-21

When I redeem a license certificate for a final license for the N9051B Pulse software, I need my HostID. Where do I find this?
On the X-Series signal analyzer, press System > Show > System. In the table, around the 10th row, you will find “HostID”, this is composed of the model and serial number.

FAQ 2014-10-21

Are trial licenses available for the N9051B Pulse Measurement Software?
Yes, a trial license is available to let you explore the N9051B free of charge for 30 days. The trial has all features enabled.

FAQ 2014-10-21

How do I upgrade to “Deep Capture” for the N9051B Pulse Measurement Software?
Deep Capture is a software license upgrade performed by the end-user. This is only available for the N9051B version, order N9051B Option 5FP.

FAQ 2014-10-21

What does the “Deep Capture” option give me in the N9051B Pulse Measurement Software?
The N9051B software operates in “batch” mode: digitizing the RF signal into IQ samples, captured a time-segment into memory, and then analyze it. Review the entire FAQ for full details.

FAQ 2014-10-21

What are key differences between N9051A and N9051B Pulse Software?
See the table in this FAQ for details.

FAQ 2014-10-21

1 2 3 4 5 6 7 8 9 10 ... Next