76-100 of 1577

Sort:
MIMO Demo Tool Install 1.2.1.msi
This demo tool provides the capability to generate multi-channel waveforms from the M9381A PXIe VSG, including waveforms and sequences of waveforms for WLAN, LTE MIMO, and Carrier Aggregation signals. This demo tool includes source code and a programming guide that can be leveraged when writing your own test code.

Programming Example 2014-05-15

FILE FILE 128.52 MB
MIMO Config Utility 1.1.6.msi
This utility assists new users in making their first measurements when using the M9381A PXIe VSG and M9391A PXIe VSA in a MIMO environment.

Programming Example 2014-05-15

FILE FILE 737 KB
E4990A Sample Programs in Help
This is sample program files which are shown in the E4990A Help. See the E4990A Help for more detail.

Programming Example 2014-05-15

ZIP ZIP 287.84 KB
[Method of Implementation] SATA SI Compliance Test

Programming Example 2014-04-28

[Method of Implementation] SATA RXTX Impedance Compliance Test

Programming Example 2014-04-28

[Method of Implementation] Ethernet Tx/Rx Return Loss Test

Programming Example 2014-04-27

E5071C-TDR State file for 10GBASE-KR/40GBASE-KR4 Tx/Rx Return Loss Tests (Option 280, 480, 285, 485)

Programming Example 2014-04-21

ZIP ZIP 1.45 MB
VBA project file for 10GBASE-KR/40GBASE-KR4 Ethernet Interconnect Tests

Programming Example 2014-04-21

ZIP ZIP 22 KB
E5071C-TDR State file for 10GBASE-KR/40GBASE-KR4 Tx/Rx Return Loss Tests (Option 2D5, 4D5, 2K5, 4K5)

Programming Example 2014-04-21

ZIP ZIP 1.53 MB
E5071C-TDR State file for 10GBASE-KR/40GBASE-KR4 Ethernet Interconnect Tests (Option 4K5)

Programming Example 2014-04-21

ZIP ZIP 5.42 MB
[Method of Implementation] MIPI M-PHY TxRx Interface S-parameter and Impedance Test

Programming Example 2014-04-08

E5071C-TDR MIPI M-PHY Tx/Rx Interface S-Parameter and Impedance Test Package
This package includes the E5071C-TDR state files and vba macro software that support the measurements described in the MOI.

Programming Example 2014-04-08

ZIP ZIP 1.55 MB
Programming Examples by Instrument
.... helping you get up and testing fast

Programming Example 2014-04-07

HDMI Source/Sink Impedance Test

Programming Example 2014-03-31

Sample application test library for Thyristor Measurement
Sample application test library to measure typical electrical characteristics of Thyristor

Programming Example 2014-03-30

ZIP ZIP 251 KB
e506162atest.exe
E5061A, E5062A Source Output Power Adjustment and Verification - VEE Program. Requirement: VEE Runtime Edition. Operating system: Windows XP or Windows 7.

Programming Example 2014-02-20

EXE EXE 355 KB
E5063A Sample Programs in Help
This is sample program files which are shown in the E5063A Help. See the E5063A Help for more detail.

Programming Example 2014-02-01

[VBA Sample Program] High Resistance Measurement for B2981A/83A/85A/87A
VBA sample program for B2981A/83A/85A/87A picoammeters/electrometers to measure high resistance by forcing voltage with B2901A/02A/11A/12A SMU or B2961A/62A Power Source. Operation guide and requirements are included in the Microsoft® Excel file.

Programming Example 2014-01-26

[VBA Sample Program] Resistivity Measurement of Insulating Materials for B2985A/87A
VBA sample program for B2985A/87A electrometers/high resistance meters to measure volume and surface resistivity of insulating materials by using the16008B Resistivity Cell. Operation guide and requirements are included in the Microsoft® Excel file.

Programming Example 2014-01-26

Keysight Edit Cal
Keysight EditCal Calibration Factor Editor Package - Operating system: Windows XP or Windows 7

Programming Example 2013-12-11

ZIP ZIP 2.50 MB
Keysight VEE Pro Code Samples
These code samples demonstrate aspects of Keysight VEE Pro programming.

Programming Example 2013-11-17

LabVIEW Programming Example: Building Arbitrary Waveforms
This example shows how to generate voltage waveforms using the list mode capability in the APS N7900 Series power supplies. The ZIP file contains a LabVIEW example.

Programming Example 2013-10-01

ZIP ZIP 27 KB
E5071C-TDR State file for 100BASE-TX Ethernet Cable Tests (Option 440, 445, 460, 465, 480, 485)

Programming Example 2013-09-24

ZIP ZIP 36 KB
E5071C-TDR State file for 100BASE-TX Ethernet Cable Tests (Option 4D5, 4K5)

Programming Example 2013-09-24

ZIP ZIP 46 KB
MATLAB Programming Example: Building Arbitrary Waveforms
This example shows how to generate voltage waveforms using the arbitrary waveform and list mode capability in the APS N7900 Series power supplies. The ZIP file contains MATLAB example and SCPI commands in a text file.

Programming Example 2013-08-28

ZIP ZIP 5 KB

Previous 1 2 3 4 5 6 7 8 9 10 ... Next