By Topic

By Industry/Technology

By Type of Content

By Product Category

201-225 of 8021

Sort:
How does the Microsoft end of support for Windows XP affect my ENA?
As of April 8, 2014 Microsoft has ceased supporting the Windows XP operating system. This document will help you answer some important questions.

FAQ 2015-07-27

Signal & Spectrum Analyzer Benchtop/Handheld Firmware Update Center
To access the most recent version of firmware or software for signal and spectrum analyzer - benchtop and handheld models.

FAQ 2015-07-09

Why doesn't my instrument showup in my application?
In I/O libraries 17.x instruments need to be added to your favorites in order for them to showup in instrument applications.

FAQ 2015-06-20

How do I upgrade my E4991B Impedance Analyzer?
Information for hardware and software options upgrade

FAQ 2015-06-19

How should I set the "Adapter Setting" of the 4294A when using the 16089A/B/C/D/E?
Please set to "NONE".

FAQ 2015-06-09

Where can I find software downloads and licensing information for Keysight EEsof EDA products?
For software downloads and licensing information, first select a product, then click the Details & Downloads button under the Trials & Licenses tab.

FAQ 2015-06-05

Does the M9290A CXA-m PXIe signal analyzer offer a tracking generator?
Yes, M9290A CXA-m has optional tracking generator function.

FAQ 2015-06-04

Can I recover the E7515A operating system if it fails to start correctly?
Yes, E7515A has an Instrument Image Recovery mode. Click on the question above for a fuller description.

FAQ 2015-05-15

Application Software for Oscilloscopes
Directs you to oscilloscope application software downloads and trial licenses.

FAQ 2015-04-29

How do I upgrade my N5182B MXG X-Series RF Vector Signal Generator?
Find Information on hardware upgrades, instrument firmware and more.

FAQ 2015-04-22

Upgrading 89600 VSA Software
Adding new options, upgrading to new revisions, and adding additional applications is described in this document.

FAQ 2015-04-21

Why doesn’t my instrument’s Java Browser Web Control work on Chome 42+?
Chrome 42 disabled the mechanism that the Java plugin uses to run in Chrome. You can use the following instructions to re-enable this until September 2015...

FAQ 2015-04-17

Why doesn’t my instrument’s Browser Web Control work?
Java security settings have been tightened and might need configuration...

FAQ 2015-04-17

How do I upgrade my PSA Series Spectrum Analyzer?
Find information on Hardware Options, Measurement Personalities, Connectivity Methods, Firmware Upgrades, etc…

FAQ 2015-04-06

Can I measure VSWR, return loss and DTF with my handheld spectrum analyzer?
Yes, the HSA N9342C handheld spectrum analyzer with option CA7 and TG7 support to read VSWR.

FAQ 2015-03-17

Industry Primary Impedance Measurement System (iPIMMS) – What is it?
In 2005 Keysight Technologies' facility at South Queensferry in the United Kingdom was the first calibration laboratory to be granted ISO/IEC 17025 accreditation for an internet-enabled technology to make measurements of complex reflection and transmission coefficient parameters.

FAQ 2015-03-16

Can I use a Windows 7 PC to upgrade my PSA Series Spectrum Analyzer?
In Windows 7 you can use the Windows XP mode to run the PSA Firmware Update Program.

FAQ 2015-03-12

How can I make 75 Ω measurements using the ENA?
You can make 75 Ω measurements with the ENA by shifting system characteristic impedance to 75 Ω.

FAQ 2015-03-09

What is the difference between the V-Applications and the Y-Applications?
The Y-Apps include the ability to run an unlimited number of waveforms for the technology purchased. The V-Apps allow waveform playback based on installation of waveform license “packs” of 5 & 50 licenses.

FAQ 2015-02-27

Do Y-Applications give me direct connectivity between Signal Studio and my EXM?
Direct connectivity from Signal Studio to the EXM is coming in a future release.

FAQ 2015-02-27

Can Y-Applications and V-Applications co-exist on the same E6640A EXM?
Yes, you may have both Y-Apps and V-Apps on the same EXM.

FAQ 2015-02-27

Is there a 3D model of the InfiniiVision 2000/3000/3000T X-Series oscilloscopes?
Yes, see the IGES, SAP, and Step format file downloads.

FAQ 2015-02-18

Keysight License Manager reports an “unspecified” Host ID and states that the Keysight license service is not running. How can I find my Host ID?
You need to install the software application you want to license on the PC...

FAQ 2015-02-10

What's new in Command Expert 1.4 and Update 1
The new features are: Improved Excel Add-on, IVI-C support, automatic instrument discovery.

FAQ 2015-02-07

IO Libraries Suite: What is Interactive LXI?
The Keysight LXI Event Explorer provides tools for creating/monitoring LXI events. The LXI Timing Explorer provides tools for monitoring the IEEE 1588 PTP clocks (setting time, selecting the system Master Clock, etc.).

FAQ 2015-02-07

Previous 1 2 3 4 5 6 7 8 9 10 ... Next