이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

VXI 메인프레임과 컨트롤러

모델 번호 입력:

1-25 / 54

정렬방식:
The trigger signals between the E1476B and the external voltmeter need to be routed through the E8491B. Can you provide the commands for the routi...
The trigger path between the external voltmeter and the E1476A is channeled through the E8491B...

FAQ 2013-01-04

IO Libraries Suite: Can I use VXI on a 64-bit OS?
IO Libraries Suite 16.1 (or later) supports VXI (E8491A/B and E1406A) on 64-bit Vista, 7, Server 2008 R2...

FAQ 2012-10-10

VEE : 왜 GPIB Address가 21번으로 설정된 장비와 통신할 수 없습니까?

FAQ 2010-09-09

IO Libraries Suite: How do I install the E8491 driver when I upgrade from a previous release to IO Libraries Suite 15.1?
Follow these steps...

FAQ 2009-08-25

E8491B: What is the part number for the Option 001 PCI FireWire Card and will other PCI Firewire cards work?
Order Part No. E8491. This is the Solectron PCI FireWire Card. The power cable is Part No. E8491-61613.

FAQ 2006-06-09

How can I reduce fan noise on a Keysight E1401B/E1421B?
To lower the fan speed, follow these instructions:

FAQ 2005-12-20

How is the E1406A memory configured from the factory?
The memory is configured into Flash and RAM memory.

FAQ 2005-08-29

How Do I Access the A32 Memory Space of VXI Through an E1406A?
Situation: The E1406A cannot access the A32 memory space of VXI. It is also limited, as permitted by the VXI specification, to only accessing the 0x200000 to 0xDFFFFF portion of A24 space.

FAQ 2005-08-23

E8491A PCI 카드를 신형 E8491B PCI 카드로 대체하고자 합니다. 아울러 E8491A의 전면판 및 E8491A와 제공되는 원래 케이블을 신형 lock-in-place 케이블로 대체하고 싶습니다. 주문해야 하는 부품 번호는 무엇입니까?

FAQ 2005-05-25

E8491B와 제공되는 원래 4.5m 케이블보다 긴 IEEE-1394(Firewire) 케이블을 사용할 수 있습니까?
길이를 추가해야 하는 경우 15개의 추가 케이블을 시스템에 추가할 수 있습니다.

FAQ 2005-05-18

Choosing between E1406A Command Module and E8491B Firewire
E8491B Firewire is faster, but E1406A is more universal.

FAQ 2004-11-08

How do I address VXI modules when using the E1406A Command Module?
Scenario: I do not understand how to address the VXI cards in my system. To address VXI cards in a system that is using a E1406A as the slot 0 controller, GPIB address must be specified with secondary addresses.

FAQ 2004-08-09

E8401A: What is the manual part number for Model E8401A?
The part number is E8401-9000.

FAQ 2004-06-28

E1401B: What is the Part Number for filler panels for the Model E1401B?
The choice of Model E1401B filler panels are: E1400-00203, E1400-00204, and E1400-00209.

FAQ 2004-06-28

What are the Rack Mounting part numbers for the E8408A?
The E8397A plus an 1494-0413 slide or E3663A rail.

FAQ 2004-06-28

E8491B/E1406A/E9851A: Differences between the SYSFAIL and FAIL LEDs on VXI Slot Controllers
SYSFAIL is usually tied to the backplane SYSFAIL line, and indicates the state of this backplane line. It will be asserted at power-on by all devices in the system and should go off when the devices pass their internal self-tests.

FAQ 2004-06-28

What are the sizes and weights of the E8401A, E8403A, and E8404A?
Size and weight information is listed in Appendix A of the E8401A, E8403A User and Service manual.

FAQ 2004-06-28

What are the meanings of the LED's on the E8401A, E8403A, and E8404A?
A solid green led is good, a flashing amber led indicates a failure.

FAQ 2004-06-28

E1406A: Is there a way to control the E1406A from a LAN connection?
Use the E5810A LAN to GPIB converter.

FAQ 2004-06-15

What is the difference between the old and new E1406A?
New E1406As have surface mount boards and maximum memory.

FAQ 2004-05-24

E1406A: Why might Model E1406A drivers disappear?
The drivers are in RAM and the battery voltage is low.

FAQ 2004-04-01

How to establish a multi-frame C-size VXI system.
Each frame is independant with its own slot 0 device (i.e. E1406A,E8491B) and unique address.

FAQ 2004-02-05

E1401B: What is the part number for a replacement power supply for the Model E1401B?
E1401-69203 refurbished, 0950-3704 new.

FAQ 2004-02-03

E1300B: What is the difference between "Peak" and "Dynamic" current in a VXI mainframe?
Peak current is DC. Dynamic current is at 10 khz.

FAQ 2004-02-03

Is PCMCIA for FireWire, E8491B, available?
Yes, please visit the IO Libraries support of IEEE 1394 CardBus Cards.

FAQ 2002-10-07

1 2 3 다음