Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

PXI Products

Support by Product Model Number:

1-25 of 128

Sort:
What is Keysight's Windows 7 to Windows 10 Migration Schedule?
We are beginning the transition of our Windows based instruments from Windows Embedded Standard 7 to Windows 10 IoT Enterprise. Click on the link for additional information.

FAQ 2017-08-07

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced TDD?
The X-Series upgrade path to LTE-Advanced TDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

Does M9393A work without M9300? If so, when using the M9393A with 100MHz reference on a pulse generator, what is the external reference input voltage?
When replacing the M9300 with a pulse generator, self-test and alignments may pass. Click on the question for additional information.

FAQ 2017-06-28

How many carriers can the MXG support in Carrier Aggregation mode?
One MXG can support one instance of the Carrier Aggregation mode. One instance of the Carrier Aggregation mode supports 5 component carriers.

FAQ 2017-06-28

How do I upgrade my X-Series Signal Analyzer to LTE-Advanced FDD?
The X-Series upgrade path to LTE-Advanced FDD depends on the existing measurement applications, and also on the operating system.

FAQ 2017-06-28

Is there a PDF version available of the user guide for the M9210A? There are issues with the .chm file that is available.
No, there is not a PDF version available for the M9210A user manual. To read the .chm file, it must be downloaded and copied on the local C drive before opening.

FAQ 2017-06-28

How do I create a Mono FM Signal using N5182B MXG ARB?
You can configure N7611B Signal Studio Broadcast Radio to play a mono/FM signal.

FAQ 2017-06-28

How do you know the serial number and calibration date (Last Verification Date) of each module?
See “About NA” in the firmware or Use a tool to check the serial number and calibration date.

FAQ 2017-06-01

How can I send the modules of M9485A to Keysight?
A recommended procedure to return to Keysight is to remove all cables and send the modules independently. Sending all modules with chassis is an optional.

FAQ 2017-05-25

What is the service (repair/calibration) support strategy?
The service (repair/calibration) support strategy of the M9485A is the module level. Only defective module can be returned, if it needs repair.

FAQ 2017-05-25

How do I install the cables and adapter for the M9485A?
The installation procedure is shown in the M9485A Start Up Guide.

FAQ 2017-05-25

How many peripheral modules (M9379A, M9341A/B, M9161D, M9111A) are supported on M9485A?
M9485A supports one M9341A/B and up to 6 M9111A. There is no software limitation for M9379A and M9161D.

FAQ 2017-05-25

Signal Analyzer IVI and MATLAB Instrument Drivers
Supported models: N9000A, N9010A, N9020A, N9030A, N9038A, E4406A, E4440A, E4443A, E4445A, E4446A, E4448A, N8201A, E4447A, E4401B, E4402B, E4403B, E4404B, E4405B, E4407B, E4408B, E4411B, E7401A, E7402A, E7403A, E7404A, E7405A, M9290A, N9040B, N9038A, M9420A, N9000B, N9010B, N9020B, N9030B, N9040B, M9290A, M9420A, M9421A, SPN9026A, SPN9003A, N9041B

FAQ 2017-05-24

What is the part number of connector saver for the M9376A, M9378A/B?
The connector saver is an adapter of coaxial straight male-SMA female-SMA on the test port of the M9376A, M9378A/B. This adapter can be replaced easily if the connecter is broken or is worn down.

FAQ 2017-05-24

What is the dimension and connector location of each modules of the M9485A?

FAQ 2017-05-19

Where do I download the mechanical drawings for the Y1271A?
Files can be imported into your modeling application.

FAQ 2017-04-21

What are the similarities and differences between M9018B and M9018A?
Similarities and differences between M9018B and M9018A

FAQ 2017-03-28

Is there a 3D model of the M924xA PXIe modular oscilloscopes?
Yes, see the IGES, SAP, Step, EASM, PKG, and PDF format file downloads.

FAQ 2017-03-23

IO Libraries Suite: What is the latest version of the IO Libraries Suite?
IO Libraries Suite 2017, available online.

FAQ 2017-03-22

Where do I download the mechanical drawings for the M9005A?
Files can be imported into your modeling application.Basic dimensions and page 2 is cooling requirements

FAQ 2017-03-10

Where do I download the mechanical drawings for the M9010A?
Files can be imported into your modeling application.

FAQ 2017-02-01

Where do I download the mechanical drawings for the M9018B?
Files can be imported into your modeling application.

FAQ 2017-02-01

Where do I download the mechanical drawings for the M9019A?
Files can be imported into your modeling application.

FAQ 2016-11-16

How do I fix: unable to change GPIB settings on an M9037A or M9537A Embedded Controller?
Make the following changes...

FAQ 2016-08-27

Where do I download the mechanical drawings for the M9037A?
Files can be imported into your modeling application.

FAQ 2016-08-18

1 2 3 4 5 6 Next