Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

High-Speed Digitizers and Multichannel Data Acquisition Solutions

Support by Product Model Number:

1-25 of 44

Sort:
How do I setup for DisplayPort Hot Swap capability?
The M9537A has 3 DisplayPorts that are activated on boot-up. If you move a cable from one DisplayPort to another, you must reboot to activate the new configuration.

FAQ 2016-11-16

Where do I download the mechanical drawings for the M9502A?
Files can be imported into your modeling application.

FAQ 2016-11-16

Where do I download the mechanical drawings for the M9537A?
Files can be imported into your modeling application.

FAQ 2016-11-16

How do I make the AXIe module show up when there is an empty slot between it and the controller?
If you leave an empty slot between the M9537A controller and an AXIe module, you might not be able to use the AXIe module and an error will show up in Windows Device Manager.

FAQ 2016-11-16

How do I fix: unable to change GPIB settings on an M9037A or M9537A Embedded Controller?
Make the following changes...

FAQ 2016-08-27

Can the U4431A MIPI M-PHY protocol analyzer be controlled from an external PC via the AXIe mainframe's USB port?
Yes, the USB connected chassis option (M9502A-U20/M9505A-U20) is a viable connection strategy when using the U4431A M-PHY Protocol Analyzer instrument.

FAQ 2016-07-08

Where do I download the mechanical drawings for the M9514A?
Files can be imported into your modeling application.

FAQ 2016-01-08

Where do I download the mechanical drawings for the M9505A?
Files can be imported into your modeling application.

FAQ 2016-01-08

Where do I download the mechanical drawings for the M9521A?
Files can be imported into your modeling application.

FAQ 2016-01-08

All M9202A PXI Express 12-bit Wideband IF Digitizer IVI and MATLAB Instrument Drivers
Supported models: M9202A

FAQ 2014-08-12

L453xA: Is there any way to implement LXI class B synchronization over large areas?
The L453xA digitizer does not support LXI class B directly. However consider using...

FAQ 2014-04-07

What type of internal memory is installed into the L4532A/34A LXI Digitizers?
Please refer to the document linked to this page for a comprehensive listing of memory installed into the Keysight L4532A/34A LXI Digitizers.

FAQ 2014-04-07

Why does the chassis Soft Front Panel (SFP) not start when I connect to the chassis with my Windows XP PC?
The Keysight PXIe and AXIe chassis require Microsoft .NET Framework 3.5 SP1 installed on the PC in order for the SFP to work. Windows XP does not have this loaded automatically. If you are using a Windows XP PC, please install Microsoft .NET Framework 3.5 SP1 from Microsoft website.

FAQ 2013-07-10

Why is my M9502A or M9505A Soft Front Panel (SFP) displaying error “Unable to open instrument. Driver initialization failed.”
A 32-bit mDNS responder is required for 32-bit applications running on a 64-bit OS when using IOLS 16.2. Installing the 32-bit mDNS responder patch below will add a 32-bit mDNS responder to appropriately resolve mDNS names to an IP address for these applications.

FAQ 2012-10-10

How do you clear the M9045A, M9045B, M9047A and M9048A memory?
Please refer to the link below for the procedure on how to clear the memory for the M9045B and M9048A adapters.

FAQ 2012-05-01

What changed in the Fan Control for the M9502A and M9505A with firmware 1.3.23?
The Fan Speed parameter changed from 8-15 to 35-100.

FAQ 2012-03-27

How do you clear the M9362A-D01 memory?

FAQ 2012-01-26

Keysight Driver Migration Tool

FAQ 2012-01-20

How do you clear the M9202A PXI Express 12-bit Wideband IF Digitizer memory?

FAQ 2011-08-18

How do you clear the M9502A and M9505A AXIe Chassis memory?

FAQ 2011-07-08

Can the AC Flatness be adjusted on the L4532A / L4534A?
The AC Flatness is a characteristic that is not warranted. It is normally only adjusted at manufacturing time, however, since it was adjusted at manufacturing time it is possible to re-adjust it...

FAQ 2011-03-21

Which computers has Keysight tested with PXI or AXIe chassis?
Keysight maintains a list of tested computers...

FAQ 2011-03-14

Do these products appear in the Keysight connection expert?

FAQ 2010-10-11

Where can customers find user manuals and example programs for AXIe & PXIe products?
Datasheets of modular products will be included on the CD shipped with every product and will be available on Keysight.com from the product page...

FAQ 2010-10-06

What is the difference between AXIe 1.0 and 3.1?
The AXIe 1.0 specification is a base-level standard for "general-purpose" applications...

FAQ 2010-10-06

1 2 Next