Sprechen Sie mit einem Experten

Technical Support


Find by Product Model Number: Examples: 34401A, E4440A

76-100 of 414

In the programming for the U2701A and U2702A Modular Oscilloscopes, why do I sometimes get a different waveform…
In programming the U2701A/U2702A Modular Oscilloscopes, the waveform is different from the Measurement Manager's (AMM) because....

FAQ 2010-08-09

How can I prevent a loading delay when using the Measurement Manager with Microsoft® .NET 2.0 on a computer that is connected to a LAN…
To prevent a loading delay when using the Measurement Manager (AMM) with Microsoft® .NET 2.0, follow the instructions below:….

FAQ 2010-08-09

Why does the pulse shape of my scope probe compensation look different from the pulse shape shown…
The compensation signal (square wave) that you see is different from the pulse shape shown in the U1602A/U1604A's user’s manual because….

FAQ 2010-08-09

Why does the new U1571A battery pack for my U1602/4A Handheld Oscilloscope last less than the stipulated 4 hours…
The new U1571A battery pack of the U1602A or U1604A Handheld Oscilloscope lasts less than 4 hours because….

FAQ 2010-08-08

When will Keysight USB modular instruments and USB Modular DAQs supports Windows 7?
For 32 bit Windows 7, the supportability of modular instruments and DAQs will happen...

FAQ 2010-07-18

How do I convert *.svw file to *.csv file in PC Link for U160xA/B?
1) From within PC Link, click on the "Load SVW" icon on the tool bar...

FAQ 2010-07-18

What replaceable parts are available for the E5383A 17-channel single-ended flying lead set?
The lead set, IC clips, probe leads, ground leads, and common (long) ground leads are available for individual purchase.

FAQ 2010-07-02

What is the use model? Charge as much as possible or let it run down, then charge all the way up?
It’s not necessary to run all the way down like NICAD battery.

FAQ 2010-07-02

I have purchased the Segmented Memory option, N5454A, for my InfiniiVision oscilloscope. However, I can’t find the feature in the menus. What can I...
You need to upgrade your oscilloscope to the latest firmware...

FAQ 2010-07-02

I misplaced the scope’s hostname, what would I do to reset the hostname?
To reset the hostname, follow these instructions.

FAQ 2010-07-02

In the user calibration of InfiniiVision 5000/6000/7000 Series oscilloscopes, what accessories are needed, and what is the procedure?
Here are the required accessories, and the procedure is at ...

FAQ 2010-06-08

What replacement parts and accessories are available for the 113xA-series InfiniiMax probes?
The best place to find this information is in the most recent revision of the InfiniiMax Active Probes User´s Quick Start Guide.

FAQ 2010-06-07

How do the :MEASure:SENDvalid and :MEASure:STATistics commands affect my Infiniium's measurement results?

FAQ 2010-05-16

Keysight Infiniium Oscilloscopes: Why does the display go off screen when I lower the V/Div?

FAQ 2010-05-16

Infiniium Oscilloscopes: SCPI compliance

FAQ 2010-05-16

Active Probes and Active Probe Power

FAQ 2010-05-14

Can I program a waveform captured by my oscilloscope into a Keysight arbitrary waveform generator?
Yes. The free IntuiLink Waveform Editor software will download waveform data from Keysight Infiniium, 6000 series, and 54600 series oscilloscopes and send the data to the a Keysight 33120A, 33210A, 33220A, or 33250A generator.

FAQ 2010-05-14

What is the equivalent circuit for the 1161A 10:1 passive probe for Infiniium scopes?
The following is an approximation of the equivalent circuit.

FAQ 2010-03-17

Are there other resources for my DC power supply product questions?
Keysight's discussion forums at https://forums.tm.keysight.com/ contain tips, discussions and programming examples from other users.

FAQ 2010-03-10

My InfiniiMax probe fails calibration or does not accurately pick up the cal signal when I use the E2655A test fixture. What could be wrong?
The first step in troubleshooting a failed probe calibration should be to compare the actual signal and the probed signal. If the probed signal does not track the actual signal well, it is most likely due to a poor connection.

FAQ 2010-03-09

Keysight Infiniium Oscilloscopes: Programming the Oscilloscope
Use the example programs and programming manual available for download from this web site.

FAQ 2009-12-11

How do I get the maximum available memory depth from my Infiniium oscilloscope?
The various Infiniium models offer between 32K and 128M points of memory per channel. The following guide shows you how to get the maximum available memory from your particular scope.

FAQ 2009-11-19

I've written my own text format for SCPI in *.txt. How do I use these for SCPI completion within VEE 9.0. What tool should I use?
You can use the tool found within Keysight.com. Just search using the keyword "Keysight VEE SCPI...

FAQ 2009-11-12

VEE 9.0 has SCPI completion. How do I make my own SCPI command built-in with VEE?
Please refer to the attached Microsoft Word document for a step by step explanation...

FAQ 2009-11-12

Where to find the USB modular scopes IVI-COM programming guide?
download the programming guide.

FAQ 2009-09-29

Previous 1 2 3 4 5 6 7 8 9 10 ... Next