Here’s the page we think you wanted. See search results instead:

 

Contact an Expert

Technical Support

Wireless Device Test Sets & Wireless Solutions

Support by Product Model Number:

26-50 of 335

Sort:
How do I make measurements with the 8960 (E5515C/E)?
Keysight 8960 Online User's Guides

FAQ 2013-01-18

How do I get the manuals and release notes for the 8960 (E5515C/E)?
Online User's Guide Index

FAQ 2013-01-18

Why must my N4010A instrument firmware be A.05.06.02 (or newer)?
This is the minimum firmware revision for a hardware change that was introduced during October 2012

FAQ 2012-10-30

EXT Wireless Communications Test Set Trial Licensing FAQs

FAQ 2012-08-01

How do I upgrade my E6607B Wireless Communications Test Set?
Find Information on Hardware Options, Measurement Applications, etc....

FAQ 2012-08-01

Does 89600 VSA software (89601) support the Bluetooth® Difference Error Vector Magnitude (DEVM) test?
The 89601 Option AYA does not provide DEVM results for Bluetooth basic measurement. Keysight recommends using N9081A Bluetooth measurement application.

FAQ 2012-03-27

Is a W-CDMA Test uSIM included with the W-CDMA TA and LA?
The W-CDMA Test uSIM is included with the E6703C W-CDMA Lab Application. It is not included with E1963A Test Application.

FAQ 2012-03-02

How does the 8960 & E1961A AMPS/136 Mobile Test Application compare to the 8920B?
This comparison table indicates the ....

FAQ 2012-03-02

Can or will the N9081A and W9081A support Bluetooth® 4.0?
Yes, the N9081A and W9081A support the low energy measurements enabled by Bluetooth 4.

FAQ 2012-03-02

Why is the measured PCS band PvT mask position -6 dBc for -10 us, Mobile Station Transmit power levels 11-15, instead of following the ETSI 11.10 s...

FAQ 2012-03-02

What 8960 settings might I need to change from the default power-on state to get my W-CDMA mobile to connect on a call?
W-CDMA is a very flexible technology that requires the UE firmware, 8960 settings, and uSIM values to be consistent. If you are experiencing difficulty with Location Update, Authentication, or Call Connection, try some of these settings, one at a ...

FAQ 2012-03-02

Is there an advantage when purchasing the E6569 WTM Suite over purchasing the individual products separately?
The price of the suite is much lower than purchasing all the WTM separately. The other difference is that the Suite is licensed for a single PC and ships with one security key. More...

FAQ 2012-03-01

Why must my N4010A instrument firmware be A.05.04.01 (or newer)?
This is the minimum firmware revision for a hardware change that was introduced during December 2011.

FAQ 2012-02-24

In Help, why are some features not documented? There are also some screenshots of the User Interface in Help that do not match my WTM.
Do you have more than one WTM loaded on your PC? Did you install an older WTM after the newer version? This can overwrite Help and Language Table files. More...

FAQ 2012-02-24

Why does the Bluetooth® ACP measurement take 15 minutes to complete?
The time needed for the ACP measurement is due to the requirements of the Bluetooth-test specification.

FAQ 2012-01-10

Can the Keysight X-Series signal analyzer with N9081A Bluetooth® measurement application measure Bluetooth hopping signals?
The short answer for this question is “no”. Fundamentally, frequency hopping is needed for testing the functional capability of the Bluetooth device.

FAQ 2012-01-10

Why is the peak power for Transmit Analysis 3.78 dBm, but with Zero span it is 3.66 dBm?
It is measured in the IQ domain, not in power domain, so there is no VBW function. The most important factor is the bucket width.

FAQ 2012-01-10

When does the BER test apply in the N9081A Bluetooth® measurement application?
The BER test only applies for EDR with a PRBS9 signal pattern.

FAQ 2012-01-10

How do I repair the E6621A measurement application if it fails to launch?
A utility is available that will fix the E6621A measurement application. Click on the question above for a fuller description.

FAQ 2011-12-23

Can I recover the E6621A operating system if it fails to start correctly?
Yes, E6621A has a System Software Recovery mode. Click on the question above for a fuller description.

FAQ 2011-12-21

Can I purchase external cables for my N4011A?
Yes. Click on the question above for a fuller description.

FAQ 2011-11-30

Why are my N4010A DEVM test results different with firmware revision A.05.03.15?
Revision A.05.03.15 was a short-lived release that used a modified measurement algorithm. Please upgrade to revision A.05.03.16, which uses the correct measurement algorithm.

FAQ 2011-02-18

Drive Test: What is the Default Datum Used by the E74xx?

FAQ 2010-11-11

How do I know my N4010A can support 40MHz Bandwidth?
You can check it thru the front panel. Click on the question above for a fuller description.

FAQ 2010-11-09

Why does my E6651A fail Source Modulated Power Level Accuracy in TME?
This may be due to a compatibility issue between the E6651A firmware version and TME.

FAQ 2010-10-14

Previous 1 2 3 4 5 6 7 8 9 10 ... Next