By Topic

By Industry/Technology

By Type of Content

By Product Category

226-250 of 8029

Sort:
Can I use a Windows 7 PC to upgrade my PSA Series Spectrum Analyzer?
In Windows 7 you can use the Windows XP mode to run the PSA Firmware Update Program.

FAQ 2015-03-12

How can I make 75 Ω measurements using the ENA?
You can make 75 Ω measurements with the ENA by shifting system characteristic impedance to 75 Ω.

FAQ 2015-03-09

What is the difference between the V-Applications and the Y-Applications?
The Y-Apps include the ability to run an unlimited number of waveforms for the technology purchased. The V-Apps allow waveform playback based on installation of waveform license “packs” of 5 & 50 licenses.

FAQ 2015-02-27

Do Y-Applications give me direct connectivity between Signal Studio and my EXM?
Direct connectivity from Signal Studio to the EXM is coming in a future release.

FAQ 2015-02-27

Can Y-Applications and V-Applications co-exist on the same E6640A EXM?
Yes, you may have both Y-Apps and V-Apps on the same EXM.

FAQ 2015-02-27

Is there a 3D model of the InfiniiVision 2000/3000/3000T X-Series oscilloscopes?
Yes, see the IGES, SAP, and Step format file downloads.

FAQ 2015-02-18

Keysight License Manager reports an “unspecified” Host ID and states that the Keysight license service is not running. How can I find my Host ID?
You need to install the software application you want to license on the PC...

FAQ 2015-02-10

What's new in Command Expert 1.4 and Update 1
The new features are: Improved Excel Add-on, IVI-C support, automatic instrument discovery.

FAQ 2015-02-07

IO Libraries Suite: What is Interactive LXI?
The Keysight LXI Event Explorer provides tools for creating/monitoring LXI events. The LXI Timing Explorer provides tools for monitoring the IEEE 1588 PTP clocks (setting time, selecting the system Master Clock, etc.).

FAQ 2015-02-07

How do I upgrade my E7515A UXM Wireless Test Set?
Find Information on hardware options available for the UXM.

FAQ 2015-02-05

Software for the W4630A Series DDR4 BGA Interposers and Cabling Solutions
Is common to all DDR memory solutions, and is downloadable from the logic analyzer software download web page ...

FAQ 2015-01-27

30-Day Free Trial License for Basic and Handheld Spectrum Analyzers
30-day trial license available for handheld and Benchtop Upgrade Options

FAQ 2015-01-20

8960 Test and Lab Application - Annual Contract Subscription
This page provides a single source of test and lab application software downloads for those on the Annual Contract for the 8960 test set (E6720A). If you’re not yet on the Annual Contract and would like to be, contact your local sales representative for details.

FAQ 2015-01-19

What are the login and passwords that are used on the X-Series Signal Analyzers?
There are two different login accounts: User account and Administrator account

FAQ 2015-01-13

Can I use the Fixture Simulator functions with the 2-port ENA?
Yes, but the function is limited...

FAQ 2015-01-09

Keysight Infiniium Software Update Utility
Utilities for assessing and updating your Infiniium software.

FAQ 2015-01-07

30-Day Free Trial for X-Series Measurement Applications for X-Series Signal Analyzers with Traditional UI
30-day trial license available for the X-Series measurement applications for X-Series signal analyzers.

FAQ 2014-12-19

How do I upgrade my Spectrum / Signal Analyzer?
Information to perform a spectrum analyzer upgrade or signal analyzer upgrade.

FAQ 2014-12-18

What hardware platforms are supported by the 89600 VSA and 89600 WLA Software?
The measurement hardware front ends include supported by the current version of software are listed here.

FAQ 2014-12-16

89601B VSA software and X-Series signal analyzer software compatibility matrix
Supported versions listed here

FAQ 2014-12-16

89601A Vector Signal Analysis software and X-Series signal analyzer software compatibility matrix
Supported versions listed here

FAQ 2014-12-16

What hardware platforms are no longer supported by the 89600 VSA software?
A list of discontinued hardware by version number

FAQ 2014-12-16

Where do I find 8960 Series 10 Software
The 8960 wireless technology test and lab applications can be found here.

FAQ 2014-12-12

EMPro Licensing FAQs
Frequently asked questions related to EMPro Licensing

FAQ 2014-12-11

Where can I find system requirements and supported platform information for GoldenGate?
For GoldenGate system requirements and supported platform information, refer to the Prerequisites section for your platform at http://www.keysight.comfind/eesof-goldengate-latest-downloads

FAQ 2014-12-11

Previous 1 2 3 4 5 6 7 8 9 10 ... Next