이 페이지를 찾으시나요? 추천 검색 결과 보기:

 

전문가 상담

기술 지원

전자 측정

모델 번호 입력:

상세 분류

주제별

산업/기술

분야별 검색결과

제품 카테고리별

76-100 / 8028

정렬방식:
WaferPro Express의 최신 릴리즈 및 기타 정보 탐색
WaferPro Express용 제품별 릴리즈 정보 목록

FAQ 2016-07-15

How do I setup ADS Hotkeys & Window Preferences for Layout?
Download the Advanced Design System (ADS) Layout Hotkey Mappings and Window Preferences.

FAQ 2016-07-12

In 89601B for APSK demodulation, how does the LDPC parameter affect measurements?
LPDC adds bit encoding.

FAQ 2016-07-08

What termination model (Balanced vs. Unbalanced) should I use for my M8000 BERT?
For M8000 (M8041A/51A/61A/62A) BERT data outputs, a Termination Model must be selected in the Amplifier section of the Parameters window, Balanced or Unbalanced.

FAQ 2016-07-08

In 89601B Digital Demodulation, how can we perform Pi/4 QPSK?
QPSK can be used for Pi/4 QPSK modulation analysis, but the demodulated bits will not be valid.

FAQ 2016-07-08

If I have purchased a transportable license option, can I now purchase floating license options?
Yes, transportable and floating licenses can be used at the same time.

FAQ 2016-07-08

In N7625B, how many instances of carriers and carrier aggregations do the software support?
One connected signal generator can support one instance of Carrier Aggregation mode. One instance of Carrier Aggregation can support 5 component carriers.

FAQ 2016-07-08

In VSA software, how can I export data from the coordinate transformed data that is displayed on the trace?
This can be done by copying/pasting data, or via the API.

FAQ 2016-07-08

Can the U4431A MIPI M-PHY protocol analyzer be controlled from an external PC via the AXIe mainframe's USB port?
Yes, the USB connected chassis option (M9502A-U20/M9505A-U20) is a viable connection strategy when using the U4431A M-PHY Protocol Analyzer instrument.

FAQ 2016-07-08

Why isn’t the unit being discovered by VSA software hosted inside the instrument itself?
Check to see if Keysight Technologies is returned from the analyzer as part of the *IDN query.

FAQ 2016-07-08

In 89601B, I want to know if the setting is finished. Is there a .NET equivalent of *OPC?
No, there is no equivalent *OPC command since this is typically not required. The command "Measurements.WaitForMeasurementDone" can wait for the end of the measurement.

FAQ 2016-07-08

In 89601B Vector Mode, what is the maximum Main Time length achieved?
Main Time is limited to 524288 samples.

FAQ 2016-07-08

For 89601B, can I purchase more than 1 year of VSA Software Subscription Service?
Yes, you may add multiple quantities of 89601BU-012.

FAQ 2016-07-08

34401A에서 Guard 단자 제공 여부
34401A에서 Guard 단자가 있습니까?

FAQ 2016-07-06

명령어로 전면판/ 후면판을 선택 가능 여부
SW 명령어로 전면판/ 후면판을 선택할 수 있는지요?

FAQ 2016-07-06

34401A 는 "True RMS" AC 전압 과 AC 전류 측정을 합니까?
34401A의 "True RMS" AC 전압 과 AC 전류 측정

FAQ 2016-07-06

B2900A 제어를 위해 사용 가능한 인터페이스에는 어떠한 종류가 있나요?
GPIB,LAN,USB

FAQ 2016-07-05

Does the L449XA have USB? What interfaces are built in?
LAN and GPIB are included. The 82357B USB/GPIB converter is available if you require USB.

FAQ 2016-07-05

Does the M9290A CXA-m PXIe signal analyzer offer a tracking generator?
Yes, M9290A CXA-m has optional tracking generator function. Order option T03/T07/T13/T26 according to the frequency range.

FAQ 2016-07-05

인피니엄 오실로스코프 프로브와 6000시리즈용과의 환 여부
프로브 호환 관련

FAQ 2016-07-05

Can I use the 82357A with other USB devices on my system?
Yes, the USB spec supports up to 127 USB devices. USB powered hubs (82357A requires hubs with their own power source) can be used to connect multiple USB devices.

FAQ 2016-07-05

오실로스코프를 PC처럼 사용 관련
오실로스코프를 PC 로 활용 가능한지 여부

FAQ 2016-07-05

신호안에 펄스가 없는 구간을 추가할 수 있는 방법이 있나요?
네. 펄스 패턴에 "Off Time"을 추가할 수 있으며 원하는 펄스 조건에 맞게 시간조정도 가능합니다.

FAQ 2016-07-05

만약 Windows XP를 계속 사용한다면, 앞으로 오류수정 서비스를 받을 수 있을까요?
네. Keysight는 서비스 지원종료되기 전까지는 마지막으로 판매된 Windows XP 까지 유지보수 되도록 할 것입니다.

FAQ 2016-07-05

N9040B UXA와 호환되는 외부 믹서는 어떤것이 있나요?
다른 X시리즈 시그널 어낼라이저와 동일하게 지원됩니다.

FAQ 2016-07-05

이전 1 2 3 4 5 6 7 8 9 10 ... 다음