By Topic

By Industry/Technology

By Type of Content

By Product Category

251-275 of 8029

Sort:
Explore the Newest Release of EMPro and More
List of product-specific release information for Electromagnetic Professional

FAQ 2014-12-11

Explore the Newest Release of GoldenGate and More
List of product-specific release information for GoldenGate

FAQ 2014-12-11

Is E5810B remote USB interface supported in NI MAX environment?
No. E5810B remote USB interface is not supportable in NI MAX environment. The E5810B remote USB interface only detectable in Keysight IO libraries Suite.

FAQ 2014-12-10

30-Day Free Trial for X-Series Measurement Applications for Wireless Test Sets
30-day trial license available for the X-Series measurement applications for Wireless Test Sets.

FAQ 2014-12-08

How do I upgrade my N9020B MXA Signal Analyzer?
Find Information on Hardware Options, Measurement Applications, etc....

FAQ 2014-12-06

N7800A Test Management Environment (TME) Software
If you perform calibration for instruments owned by your company and do not offer calibration as a commercial service, you may be eligible for licensed access to Keysight calibration software.

FAQ 2014-11-26

Is U2700A series USB Modular Instruments supported in Linux environment?
No. U2700A Series are not supportable in Linux environment. The drives for USB Modular only build for Microsoft Windows.

FAQ 2014-11-25

How do I upgrade my M9290A CXA-m PXIe Signal Analyzer?
Find Information on Hardware Options, Measurement Applications, etc....

FAQ 2014-11-17

How do I upgrade my E6650A EXF Wireless Test Set?
Find Information on Hardware Options, Measurement Applications, etc....

FAQ 2014-11-10

How do I find my Host ID when I run software on a PC?
For the PSA model, when requesting an N9051A trial

FAQ 2014-10-31

Where do I find E6651A Mobile WiMAX™ Test Set Software and Firmware
Links to N64xxA and E665xA software and the neccessary firmware.

FAQ 2014-10-28

VVM measurement with E5061B for replacing 8508A vector voltmeter

FAQ 2014-10-22

PDF PDF 381 KB
If I have N9051A Pulse Measurement Software, how do I upgrade to N9051B?
Order N9051B Option A2B to receive a user-installed software license, which causes any existing N9051A licenses to be recognized as N9051B licenses. The N9051B-2FP license is required, while all others are optional and independent of each other.

FAQ 2014-10-21

How is the N9051B Pulse Measurement Software delivered, installed and licensed?
Important: N9051B runs only on the CPU inside an X-Series signal analyzer, which must be Windows 7 and 64-bit. See the FAQ for further details.

FAQ 2014-10-21

Are trial licenses available for the N9051B Pulse Measurement Software?
Yes, a trial license is available to let you explore the N9051B free of charge for 30 days. The trial has all features enabled.

FAQ 2014-10-21

What are key differences between N9051A and N9051B Pulse Software?
See the table in this FAQ for details.

FAQ 2014-10-21

How does the N9051B Pulse Measurement Software GUI work?
The GUI is standard MS Windows type: pull-down menus, dialogs, on-screen buttons, etc. A USB mouse and keyboard are required. The PC-ststandard keys of the X-SA front panel are recognized: numbers (digits 0-9, decimal point, minus, BkSp); plus Enter, Select, Escape, Ctrl, Alt, Del, and Tab; and the Mode key.

FAQ 2014-10-21

I ordered the N9051A, but it is no longer installed on the signal analyzer. The N9051B is installed, but my N9051A licenses don’t work. What shou
The N9051B is the recommended replacement for N9051A. The N9051A license can be upgraded by adding a low-cost N9051B-A2B license.

FAQ 2014-10-21

What does the “Deep Capture” option give me in the N9051B Pulse Measurement Software?
The N9051B software operates in “batch” mode: digitizing the RF signal into IQ samples, captured a time-segment into memory, and then analyze it. Review the entire FAQ for full details.

FAQ 2014-10-21

How do I upgrade to “Deep Capture” for the N9051B Pulse Measurement Software?
Deep Capture is a software license upgrade performed by the end-user. This is only available for the N9051B version, order N9051B Option 5FP.

FAQ 2014-10-21

When I redeem a license certificate for a final license for the N9051B Pulse software, I need my HostID. Where do I find this?
On the X-Series signal analyzer, press System > Show > System. In the table, around the 10th row, you will find “HostID”, this is composed of the model and serial number.

FAQ 2014-10-21

How do I upgrade my N5172B EXG X-Series RF Vector Signal Generator?
Find Information on hardware upgrades, instrument firmware and more.

FAQ 2014-10-14

How can I determine what CPU shipped with my PXA, MXA, or EXA?
CPU install details can be found here...

FAQ 2014-10-13

How does the Microsoft end of support for Windows XP affect my M9036A?
In Keysight’s ongoing efforts and commitment to provide the best possible product quality and improve the overall customer experience with our M9036A PXIe Embedded Controller, we would like to inform you that we have made the conscious decision to not migrate the XP version of the M9036A to Windows 7.

FAQ 2014-10-12

What is the bandwidth of the wideband I.F. output of the N9040B UXA signal analyzer?
Same as the N9030A PXA signal analyzer with Option CR3, wideband IF output.

FAQ 2014-10-06

Previous ... 11 12 13 14 15 16 17 18 19 20 ... Next