By Topic

By Industry/Technology

By Type of Content

By Product Category

101-125 of 8020

Sort:
What comes standard or pre-configured in my NFA X-Series analyzer and what options are available at the time of initial purchase?
See the list by selecting the link...

FAQ 2016-04-08

Why doesn't the 16195B have calibration data?
The 16195B contains Open, Short, 50 Ω Load and Low-loss Capacitor terminations for calibrating the 4287A, E4982A, E4991A, E4991B and E5061B.

FAQ 2016-03-31

What is the phase noise sensitivity of the E5052B with E5053A and 11970 Mixers?
Please refer to this document.

FAQ 2016-03-29

Where can I find PNA/PNA-L/PNA-X Upgrade Options detail?
This is the link to the CTD external server for PNA family Upgrade option detail

FAQ 2016-03-28

N9000AK Option R2C, Revise to Current Information
N9000AK Option R2C, Revise to Current Information

FAQ 2016-03-22

N9010AK-R2C and N9020AK-R2C, Revise to Current Information
N9010AK-R2C and N9020AK-R2C, Revise to Current Information

FAQ 2016-03-22

E8257D and E8267D Option R2C, Revise to Current Information
What option R2C provides

FAQ 2016-03-22

Where can I find PNA/PNA-L/PNA-X Firmware, Software and Support information?
This is the link to the CTD external website for PNA Firmware, Software, and other support information

FAQ 2016-03-22

N9030AK Option R2C, Revise to Current Information
N9030AK Option R2C, Revise to Current Information

FAQ 2016-03-22

Can I make my golden sample’s characteristic trace as the limit for others?
Yes

FAQ 2016-03-17

Does N9322C offer window limit as the N9320B’s?
Yes

FAQ 2016-03-15

Can N9322C record spectrum over time?
Yes

FAQ 2016-03-15

What is the band power measurement?
band power

FAQ 2016-03-15

What does channel scanner do?
measures channel power

FAQ 2016-03-15

Does N9322C provide CISPR filters and quasi-peak detector?
Yes

FAQ 2016-03-15

Does N9322C offer trial license for its measurement features?
yes

FAQ 2016-03-15

How to edit amplitude correction factor?
correction factor

FAQ 2016-03-15

Does N9322C support AM/FM tune and listen?
yes

FAQ 2016-03-15

In the channel scanner mode, are there any pre-defined standards?
yes

FAQ 2016-03-15

Does N9322C provide CISPR band presets?
Not exactly

FAQ 2016-03-15

Does N9322C support security feature?
yes

FAQ 2016-03-15

What does “FSK error” mean in option DMA (ASK/FSK demodulation analysis)?
modulation signal quality

FAQ 2016-03-15

When will the X-Series signal analyzers and the One Box Testers (OBT's) migrate to Windows 10?
No dates have been set, support for Win7 end October, 2020...

FAQ 2016-03-14

What measurement applications can I install on my NFA X-Series Noise Figure Analyzer?
Short list can be found here...

FAQ 2016-03-03

Does 34450A supports multiple measurements per trigger event?
No.

FAQ 2016-02-29

Previous 1 2 3 4 5 6 7 8 9 10 ... Next