Voici la page que nous pensons que vous vouliez. Voir les résultats de la recherche au lieu:

 

Discutez avec un expert

Support technique

Mesure Electronique

Support by Product Model Number:

Affiner la liste

retirer tout le raffinement

Par industrie/technologie

Par type de contenu

Par catégorie de produit

Par autre catégorie

451-475 sur 991

Tri:
Agilent Technologies Introduces 6-GHz Signal Generators with Industry-Best Performance
Today's aerospace/defense environment requires enhanced radar performance to detect weak signals at long distances. To provide the pure and precise signals needed to test these designs, the MXG uses an innovative triple-loop synthesizer to deliver phase noise performance of -146 dBc/Hz at 1 GHz and 20 kHz offset. For developers of radar components such as mixers and analog-to-digital converters, the MXG also features industry-leading spurious performance of -96 dBc at 1 GHz.

Dossier de presse 2012-05-01

Agilent to Acquire Centellax’s Test and Measurement Business
Agilent Technologies Inc. (NYSE: A) and Centellax today announced they have signed a definitive agreement for Agilent to acquire the assets of Centellax's test and measurement business.

Dossier de presse 2012-04-27

Agilent Technologies Named Oscilloscope Company of the Year
The award is based on Frost & Sullivan's recent analysis of the oscilloscope market.

Dossier de presse 2012-04-26

Agilent Technologies’ Advanced Design System Selected by Comtech EF Data for Satellite Communication
...a clear-cut advantage compared to other tools we had evaluated,” said Tibi Artzi, unit manager with Comtech EF Data

Dossier de presse 2012-04-25

ADS Selected by Comtech EF Data for Satellite Communications, High-Frequency Power Amplifier Design
Agilent announces that Comtech EF Data, a subsidiary of Comtech Telecommunications Corp., has selected ADS for use in developing RF and microwave circuits for high-performance satellite communications systems.

Dossier de presse 2012-04-25

Agilent Technologies Named Oscilloscope Company of the Year
The award is based on Frost & Sullivan's recent analysis of the oscilloscope market. Frost & Sullivan ranked Agilent as the No. 2 company in 2009, but its rapid revenue growth since then has made it the leader in market penetration.

Dossier de presse 2012-04-25

U4324A flying lead probe: industry’s most cost-effective PCI Express 3.0 probing solution

Dossier de presse 2012-04-05

Agilent Technologies Announces Enabling 802.11ac Signal Generation

Dossier de presse 2012-03-27

Agilent Technologies Announces Bluetooth® Low Energy RF Test Solution on N4010A

Dossier de presse 2012-03-26

Agilent Announces Shipment of the IC-CAP 2012 Platform for Device Characterization and Modeling
Agilent announces shipment of the latest release of its device modeling software platform, the Integrated Circuit Characterization and Analysis Program (IC-CAP) for 2012.

Dossier de presse 2012-03-02

Agilent Technologies Introduces Wireless Link for Remote Monitoring and Data Logging with Handheld
Agilent Technologies Inc. announced the introduction of a wireless connectivity solution that links up to three Agilent handheld digital multimeters to smartphones, tablets and PCs.

Dossier de presse 2012-03-01

Electrical and Optical Clock Data Recovery Solutions
Agilent Technologies Inc. (NYSE: A) today introduced a new family of instrumentation-grade clock recovery solutions for optical and electrical testing of high-speed digital communications components and systems. The solutions offer the industry's highest bandwidth and low jitter performance at significantly lower cost than similar products.

Dossier de presse 2012-02-28

Agilent Technologies Introduces Fully Integrated Optical Modulation Analyzer for Testing 40/100G
Agilent Technologies Introduces Industry's First Fully Integrated Optical Modulation Analyzer for Testing 40/100G,

Dossier de presse 2012-02-28

Agilent Technologies Announces Test Software for Equipment Based on Altair TDD/FDD LTE Chipset

Dossier de presse 2012-02-28

Agilent's SystemVue Software Selected by Télécom ParisTech for 3G/4G Transmitter Research
Agilent announced that Télécom ParisTech, one of France's leading graduate engineering schools, has selected the company's SystemVue software for use in analog and mixed integrated systems research.

Dossier de presse 2012-02-28

Agilent's EMPro and Momentum Selected by OSAT for Next-Generation Circuit and Antenna Development
OSAT Company, which specializes in engineering analysis, testing and inspection techniques, is using Agilent’s Electromagnetic Professional software, EMPro, and the Momentum 3-D planar electromagnetic simulator to design and simulate innovative new antennas and circuits.

Dossier de presse 2012-02-24

Agilent Announces 30-Second Demo Series of User-Inspired Microwave EDA Software Innovations
Agilent announced the launch of a series of 30-second demos on 10 popular microwave EDA usability innovations for its Advanced Design System software, the industry's leading electronic design automation software for RF, microwave and high-speed applications.

Dossier de presse 2012-02-22

Agilent Completes Acquisition of Accelicon Technologies’ Solutions for Semiconductor Device Modeling
Agilent Technologies announced that Accelicon Technologies’ software solutions and technology for device-level modeling and validation in the electronics industry are now part of Agilent.

Dossier de presse 2012-02-21

Agilent Technologies' Latest Genesys Software Enhances RF System Design
Agilent announces the latest release of its industry-leading, low-cost, high-performance software for RF and microwave board design, Genesys 2012.

Dossier de presse 2012-02-16

Agilent Technologies Announces 42-Mbps DC-HSDPA IP Data Throughput Solution for the 8960 Wireless
The Agilent E5515E delivers sustained, end-to-end IP data throughput at 42 Mbps, flexible and comprehensive RF measurements, and improved hardware capability for future requirements, making it easy and fast to stress wireless devices and verify their performance at full data rates.

Dossier de presse 2012-02-14

Agilent Technologies to Demonstrate Industry-First R&D and Manufacturing Test Solutions
Agilent Technologies will demonstrate its industry-first communications test and measurement solutions for LTE-Advanced, LTE, HSPA+, dual-carrier HSDPA, MIMO, multi-standard radio and voice over LTE, along with 2G/3G solutions for R&D, manufacturing and deployment at the Mobile World Congress in Barcelona, Feb. 27- March 1.

Dossier de presse 2012-02-13

Agilent to Demo Industry-1st R&D/Mfg. Test Solutions for LTE-A, LTE & HSPA+ at Mobile World Congress
Agilent will demonstrate its industry-first communications test and measurement solutions for LTE-Advanced, LTE, HSPA+, dual-carrier HSDPA, MIMO, multi-standard radio and voice over LTE, along with 2G/3G solutions for R&D, manufacturing and deployment at the Mobile World Congress in Barcelona, Feb. 27- March 1.

Dossier de presse 2012-02-13

Agilent Technologies Chipset Software Supports picoChip Femtocell Test
Agilent Technologies Inc. (NYSE: A) and picoChip today announced a high-volume manufacturing test solution for 3G femtocell products.

Dossier de presse 2012-02-07

ETS-Lindgren Announces Support of Agilent PXT Wireless Test Set for LTE Over-the-Air Testing
Agilent PXT performs OTA tests to industry standards and allows user equipment (UE) developers to characterize and optimize the behaviour of their designs. The EMQuest/PXT solution is offered with all ETS-Lindgren AMS for the testing of wireless devices

Dossier de presse 2012-02-03

Agilent Technologies Announces Industry's First Eight-Channel RF Measurement Solution Addressing LTE
Agilent Technologies Inc. (NYSE: A) today introduced industry-leading enhancements to its N7109A multi-channel signal analyzer for emerging multichannel LTE, LTE-Advanced and MIMO RF measurement requirements, including LTE antenna beamforming and LTE-Advanced carrier aggregation.

Dossier de presse 2012-02-02

Précédente ... 11 12 13 14 15 16 17 18 19 20 ... Page suivante