这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

缩小范围

去除所有优化

行业/技术

按内容类型

按产品类别

201-225 / 797

排序:
Article – complex coding for increased optical efficiency
Article – complex coding for increased optical efficiency

文章 2013-07-22

Article – why complex modulated signals?
Article – why complex modulated signals?

文章 2013-07-22

Herding Technical Cats
Engineering degree offers more jobs than in R&D. (EETimes, 7/11/2013)

文章 2013-07-15

Microwave Journal Article: Streamlining BER Simulation and Measurement
Bit Error Rate (BER) remains the ultimate quality metric for all communication systems. Emerging 4G systems like LTE specify throughput rate as a metric for system performance. These 4G systems add intelligence by using adaptive modulation based on channel quality, but under the hood, BER is measured while the modulation is adjusted.

文章 2013-07-12

Industry Publications on X-Parameters
A number if important industry publications on X-parameters.

文章 2013-07-12

Realization and Analysis of Electronically Steerable Phased Array using Scripting & Parameterization
With the advent of multi-core, high speed processors and abundant memory availability, complex designs using 3-D full-wave electromagnetic (EM) tools have become common choice for microwave and antenna engineers.

文章 2013-07-09

Simulation and Measurement-based X-parameter Models for Power Amplifiers with Envelope Tracking
An investigation of envelope tracking power amplifiers using simulation-based and measurement-based frequency domain static XP models.

文章 2013-06-30

PDF PDF 544 KB
Using Network Analyzer Time-Domain Analysis to Verify and Troubleshoot Complex Components - Article
Microwave Product Digest May 2013 feature article that discusses using FieldFox's time domain analysis to troubleshoot complex components.

文章 2013-06-19

PDF PDF 1.60 MB
What is waveform update rate and why does it matter?
Explore this often overlooked oscilloscope performance specification to learn how to determine an oscilloscope’s update rate and what a fast update rate can mean for you.

文章 2013-06-03

University of Hawaii using Keysight Equipment for Patient Monitoring Research

文章 2013-05-27

Celebrating 100 Years of Excellence in Engineering Education and Research

文章 2013-05-27

Artificial Retina Research at the University of Utah Provides Hope for the Blind

文章 2013-05-27

Students “Learn by Doing” at Cal Poly

文章 2013-05-27

Keysight Test Equipment Hits the Ivy League

文章 2013-05-27

Keysight Equipment Plays an Instrumental Role in Prototype Alternative Breast Imaging Technique

文章 2013-05-27

Yellow Jackets Buzz at the Speed of Light

文章 2013-05-27

Keysight and ITESM (Mexico) Collaborate to Prepare Students for Careers in Industry

文章 2013-05-27

Morgan State Strives to Make Engineering Education More Accessible

文章 2013-05-27

教育计划电子期刊――2008 年 6月第 2 期
教育计划电子期刊――2008 年 6月第 2 期

内部通讯 2013-05-07

Electronic Manufacturing Test Support eNews - April 2013
Latest information to help you with ICT, 5DX and Automotive Electronics Functional Test Systems Support

内部通讯 2013-04-25

What is the difference between IEEE 802.11ac and 802.11ad?
Microwave & RF article, April 2013. The goal is for all IEEE 802.11 standards to be backward compatible and for 802.11ac and 802.11ad to be compatible at the medium-access-control (MAC) or data-link layer. They should differ only in physical-layer (PHY) characteristics. Read about how that goal is being attained.

文章 2013-04-23

Ensuring The Highest Quality Microwave Measurements - Article
High frequencies and stringent application specifications drives a number of critical challenges to be addressed in this article.

文章 2013-04-22

Incremental Redundancy in EGPRS
Incremental redundancy is implemented in EGPRS systems to achieve maximum efficiency in over-the-air interface... WirelessDesignMagazine.com article by Paul Mercy. Feb 2005. Acrobat PDF.

文章 2013-04-02

Enabling Simulation and Test of Custom OFDM Signals
Orthogonal frequency division multiplexing (OFDM) has become attractive for many current and emerging commercial applications because it provides a combination of data throughput, scalability, and robustness.

文章 2013-04-01

A Packaged 60 GHz Low-Power Transceiver with Integrated Antennas for Short-Range Communications
This paper describes a 60-GHz transceiver with integrated antennas for short range and low power wireless communications fabricated in a CMOS 65nm SOI technology.

文章 2013-03-25

PDF PDF 429 KB

以前 1 2 3 4 5 6 7 8 9 10 ... 下一页