这是我们认为您想要浏览的网页。 查看搜索结果:

 

与专家交流

技术支持

电子测量

按产品型号支持:

缩小范围

去除所有优化

行业/技术

按内容类型

按产品类别

126-150 / 797

排序:
5G 毫米波 MIMO 信道探测:技术挑战和原型系统
在本文中,我们重点讨论了如何使用商用仪器建立毫米波 MIMO 信道探测系统,破解主要技术挑战。

文章 2014-12-18

Frost & Sullivan 2014 Global Instrumentation Software Market Leadership Award – Article Reprint

文章 2014-11-14

PDF PDF 1.97 MB
Design of an 8×8 MIMO Broadband RF Subsystem for Future WLAN
Microwave Journal, November 13, 2014 article by Southeast University describes a broadband 8×8 MIMO RF subsystem with large area coverage for next generation WLAN in the 5 GHz band.

期刊 2014-11-13

Engineering Students in Brazil Learn with Hands-on Projects
Engineering Students in Brazil Learn with Hands-on Projects

文章 2014-10-28

IRCICA Creates a Telecommunications Test Platform for Industrial and Academic Research
IRCICA Creates a Telecommunications Test Platform for Industrial and Academic Research

文章 2014-10-16

AWG article - MWJ product feature
AWG article - MWJ product feature

文章 2014-10-14

MIT Lives Up to its Motto: Mind and Hand
MIT Lives Up to its Motto: Mind and Hand

文章 2014-09-21

HeatWave Case Studies
HeatWave Electro-Thermal simulation case studies.

案例分析 2014-09-18

HeatWave 技术文章
与 HeatWave 电热分析软件有关的技术文章链接。

文章 2014-08-27

Mechanism of Jitter Amplification in Clock Channels
In this paper. jitter amplification in clock channels is analyzed analytically using the techniques developed in "Frequency domain analysis of jitter amplification in clock channels."

文章 2014-08-04

PDF PDF 715 KB
Touchstone v2.0 SI/PI S-Parameter Models for Simultaneous Switching Noise (SSN) Analysis of DDR4
This article reprint presents a methodology to setup and analyze Simultaneous Switching Noise for DDR4 applications using Touchstone v2.0 models.

文章 2014-08-04

PDF PDF 8.20 MB
De-Mystifying the 28 Gb/s PCB Channel: Design to Measurement
This paper demonstrates a design methodology for 28 Gb/s SERDES channels using Xilinx Virtex-7 Tx to show the required trade-offs that enable robust performance that is easy to verify with measurement.

文章 2014-08-04

PDF PDF 2.84 MB
IBIS AMI Modeling of Retimer and Performance Analysis of Retimer based Active Serial Links
This paper presents a novel retimer modeling approach based on IBIS-AMI to capture the performance of a retimer that operates up to 15 Gbps.

文章 2014-08-04

PDF PDF 1.88 MB
Modeling, Extraction and Verification of VCSEL Model for Optical IBIS AMI
A technique of modeling and extraction of VCSEL devices for IBIS-AMI has been proposed.

文章 2014-08-04

PDF PDF 1.18 MB
FEM Modeling of Gigahertz TEM Cells for Susceptibility Analysis of RFID Products
This paper presents a novel simulation methodology to model the coupling between a GTEM cell and an RF-ID antenna.

文章 2014-08-03

PDF PDF 816 KB
In-Circuit Test (ICT): The King Is Dead; Long Live the King!
Reports of the demise of in-circuit testing have been exaggerated for at least 20 years. Despite this, ICT is still here and kicking. This paper discusses various reasons why the King lives on.

文章 2014-08-01

PDF PDF 201 KB
Surviving State Disruptions Caused by Test: A Case Study - Article Reprint
This paper discusses new instructions for IEEE 1149.1 boundary scan tests that can remove "lobotomy problems" during tests.

文章 2014-08-01

PDF PDF 3.07 MB
Intellectual property and copyright protection on Agilent ICT products
This letter advises areas of intellectual property and copyright protection to look out for when customers elect to purchase Agilent in-circuit test products from third party vendors.

专访 2014-07-31

PDF PDF 155 KB
Matching Network Yin-Yang - Part 2
This Article by Randy Rhea covers transmission line matching networks, plus a discussion of characteristics of the load affects matching bandwidth and the choice of network topologies.

文章 2014-07-31

PDF PDF 411 KB
Using S-Parameter Data Effectively
This Article by Wilfredo Rivas-Torres focuses on how to incorporate Sparameters in the design process using a CAD approach.

文章 2014-07-31

PDF PDF 248 KB
Comparing Boundary Scan Methods White Paper
The need for reusable tests is driving standalone boundary scan-ICT integration. This article first appeared in the September 2009 issue of Circuits Assembly and is reprinted with kind permission.

文章 2014-07-31

PDF PDF 2.75 MB
Matching Network Yin-Yang - Part 1
This Article by Randy Rhea covers basic matching concepts and matching network topologies, emphasizing methods for obtaining the desired performance with networks that are realizable in practice.

文章 2014-07-31

PDF PDF 554 KB
Designing RFID Tags Using Direct Antenna Matching
This Article by Cory Edelman and Murthy Upmaka describes the design challenges involved in RFID design and also focuses on the use of integrated EDA tools to optimally address the challenges.

文章 2014-07-31

PDF PDF 1.09 MB
Design and Characterization of Discontinuous RF/Microwave Passive Components
This Article by Dean Nicholson presents a design methodology proposed for designing and building RF circuits likely to contain discontinuous regions.

文章 2014-07-31

PDF PDF 1.43 MB
Symmetric and Asymmetric - Coupled Lines Band-Stop Filters at Ku/Ka Bands
This Article presents theory and design of coupled-line spur line band-stop filters, which are quite compact structures, lower radiation loss than conventional shunt stub and coupled-line filters.

文章 2014-07-31

PDF PDF 1.38 MB

以前 1 2 3 4 5 6 7 8 9 10 ... 下一页