By Topic

By Industry/Technology

By Type of Content

By Product Category

126-150 of 1163

Sort:
What is the process to capture a trace image to the floppy disk on the Keysight 8712ES/ET and 8714ES/ET Vector Network Analyzers?
The 8712ES/ET and 8714ES/ET Vector Network Analyzers support HPGL, PCX, PCL5, and GIF image saves via the floppy drive.

FAQ 2012-12-11

On the ENA 6 series, can I use Supr Avoid ON/OFF function like the 871x?
No. It is always ON.

FAQ 2012-12-11

On the ENA 6 series, can I use swept sweep mode?
No. The ENA 6 series always sweeps in step.

FAQ 2012-12-11

Do I need to perform a periodic front panel instrument alignment on my N9039A RF Preselector?
No, but there is a system alignment that needs to be periodically run. See FAQ content for details...

FAQ 2012-12-11

How often does the system user alignment for the PSA EMI Measurement Receiver need to be run?
30 days or 3° C temperature change. See contents for details...

FAQ 2012-12-11

What features are different between the ENA 7 series and the ENA 6 series?
Followings are the difference between the ENA 7 series and the ENA 6 series.

FAQ 2012-12-11

Are mixed mode S-parameter measurements possible on the 2-port ENA?
Yes. The equation editor function allows for the real-time calculation of mixed mode S-parameters on the 2-port ENA.

FAQ 2012-12-10

Does the ENA 6 series support direct sampler measurements and user ratio measurements?
No.

FAQ 2012-12-10

What Configuration issues are there with option AYQ, Quasi Peak Detector in the ESA-E Series of Spectrum Analyzers?
View the compatibility issues here....

FAQ 2012-12-05

On the Keysight E4980A, what is the "DC Source Option 001 (±10 VDC Max)" and how is it utilized?
A summary description of the enhancements provided by E4980A option 001 - 'Power and DC Bias Enhancement Option'

FAQ 2012-12-02

What you need to know about Advanced DGN Reporting?
Frequently Asked Questions about Advanced DGN Reporting.

FAQ 2012-11-28

How to debug the 3 differences that are encountered on the new hybrid pin cards (P/N: E4000-66562 and E4000-66563)?
Follow the guideline to debug your test when you start using the new bybrid pin cards: • E4000-66562 for 6MPs (standard hybrid pin card) • E4000-66563 for 12MPs (advanced hybrid pin card)

FAQ 2012-11-12

Are there any reference documents for TRL Calibration of network analyzers?

FAQ 2012-11-05

How can previously created data in BenchLink II be exported?
Open a previously saved configuration file with data and then export the data as a Text (.txt) file or Comma Separated values (.csv) file.

FAQ 2012-11-05

Can I manually set the sample rate on my InfiniiVision oscilloscope?
Although the sample rate cannot be directly set on any InfiniiVision oscilloscope, it can be set indirectly by adjusting the oscilloscopes time per division setting.

FAQ 2012-10-30

Will the external mixer Option EXM support the 11974 Series preselected mixers?
There are no plans to support the 11974 Series preselected mixers with the N9030A PXA.

FAQ 2012-10-25

Is the N9068A phase noise application supported by N9030A PXA Option EXM external mixing?
Yes, the N9068A phase noise application is supported when using N9030A PXA Option EXM external mixing. In addition, Option EXM supports normal spectrum analyzer applications, including PowerSuite one-button measurements.

FAQ 2012-10-25

Does the PXA (with Option EXM) support the 11970VE01 mixer (50 to 85 GHz)?
Yes.

FAQ 2012-10-25

Sample DLL for i3070 External DLL Feature
External DLL (dynamic- link library) call feature expands i3070 platform capability for additional functional test / application in a flexible way. Here is a DLL example of data management, updating the test status to a database.

FAQ 2012-10-18

Which Keysight oscilloscopes have a 10 MHz reference input/output?
6000 Series, 6000L Series, 7000A Series, 7000B Series, 9000 Series, 54850 Series (Output only), 80000A Series, 80000B Series, 90000A Series and 90000 X-Series

FAQ 2012-10-17

What is the difference between the Auto and Normal trigger modes on InfiniiVision oscilloscopes?
In auto trigger mode, the trigger will be forced if the specified conditions are not met. In normal trigger mode, the trigger will never be forced and a trigger will only occur if the specified conditions are met.

FAQ 2012-10-17

What external mixers will work with my PXA/mmW EXA and how do I order them?
Currently, the N9030A PXA/mmW EXA with Option EXM will work with either the 11970 Series (with the exception of the 11970K) or ) or external mixers from other vendors such a OML Inc. mixers.

FAQ 2012-10-17

XVision fails to install on some laptops
Before installing XVision /ICT software, please follow the steps below:

FAQ 2012-09-25

What is the typical power consumption of the 86100C and 86100D Digital Communications Analyzer?
Typical measurements of 86100C and 86100D power consumption

FAQ 2012-09-25

How do I get >8 bit vertical resolution on my Keysight real-time oscilloscope?
Most Keysight oscilloscopes give 8-bit vertical resolution at normal acquisition mode.

FAQ 2012-08-31

Previous 1 2 3 4 5 6 7 8 9 10 ... Next