By Topic

By Type of Content

By Product Category

1-3 of 3

Sort:
What is the frequency range of the N5532A Sensor Module?
100 kHz to 4.2 GHz, 10 MHz to 18 GHz, 30 MHz to 26.5 GHz, and 30 MHz to 50 GHz.

FAQ 2012-02-26

How can I clear a "bad disk" or "bad file name" error message when accessing the internal RAM memory on the 89441A or 89410A?
If a "bad disk" error message occurs when trying to catalog a disk, or a "bad file name" message occurs when trying to copy a disk file, the non-volatile RAM memory (NVRAM disk) in the 89410A or 89441A has become corrupted.

FAQ 2012-02-25

Can I change the regional setting of Windows system running in the E5052B?
No, the default setting is "English (United States)" and the E5052B can not support the other setting.

FAQ 2008-07-18